Page 1 of 11 12345 ... LastLast
Results 1 to 10 of 112

Thread: MorpHex, a sphere formed morphing hexapod

Hybrid View

Previous Post Previous Post   Next Post Next Post
  1. #1
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    84

    MorpHex, a sphere formed morphing hexapod

    This is a project I've been thinking on for a very long time. Shortly explained this is a sphere shaped hexapod that I plan to give the following features:

    • Roll freely like a ball
    • Have different sort of locomotion for moving in any direction
    • Variable inner-body dimensions
    • Transform from a sphere shape into a hexapod and vice versa
    • Walk like a hexapod


    Before I started to make any exact sketches or started building anything, I shared my ideas with my friend Jeroen Janssen (Xan). We talked about this project when I visited him in Netherlands this summer. At first I was thinking of using a fixed sized inner body with 6 x 4 DOF legs, similar to what I used for the T-Hex hexapod. Another problem was finding a sphere shaped material that I could use. Jeroen and I went to a local toy-shop and I just asked him to look for ball-shaped object. After a little while Jeroen had found a globe! At that moment I got the feeling that using a globe could actually work. After a few months and some searching in different book and toy-shop’s I found a 28cm in diameter globe from Toysrus. It was also cheap and the plastic material seemed to be relative solid (about 3mm thick).

    I’m cutting out 12 identical sphere parts. Using a simple handsaw and cutting along the lines of the Longitude every 60 deg. The line of equator was made of 1mm thick dark blue plastic band and was very easy to remove, that resulted in a perfect clean edge too! Here are some pictures of the sphere parts:





    The map coating was very easy to peel of. The trick was to preheat the surface carefully and then start in one corner and just peel off the whole layer. To the left is the original part. The middle part has the globe/map layer peeled off and the right part is sanded by hand:



    As you can see the material is very transparent, I do have some future ideas of mounting several LED’s for some cool lighting effects.

    Morphing inner-body:



    The principle is very simple. I’m using one digital 5645 servo in the centre of the body, the servo holds two delrin gears.





    I’m using 7x of the LPA gear sets from Lynxmotion. One gear with SES holes is mounted to each of the 6 outer body sections.



    This construction makes it possible to adjust the body dimension by about x2 using only one servo.



    The main reason for making the body like this is to hopefully make some more free space for each leg when the robot are in the walking mode. Even with the increased body size the legs are still going to be highly restricted in free motion caused by the large sphere parts, but I think it will work I've already done some changes to the body section, like replaced the 1,5 mm aluminium parts used on the 6 outer sections to 2mm for more strength and stability. And also some more stuff like an holder for electronics.

    There is still a lot of work left and I'm currently working with assembling all the legs. In total there will be 31 servos, 12* 5990 + 19*5645.

    I'll post more info when I'm finished with all the legs and have some more and better photos.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    282

    Re: MorpHex, a sphere formed morphing hexapod

    I don't like to use smileys, but .

    That seems like a pretty effective way to simultaneously stuff a hex in an even smaller sphere and reducing the sphere's interference with the bot's mobility.

    innerbreed has been working on a similar project for a while, but had to abandon the pre-made sphere.
    http://forums.trossenrobotics.com/showthread.php?t=4399

  3. #3
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    84

    Re: MorpHex, a sphere formed morphing hexapod

    Thanks!

    Yeah I'm very aware of Jonny's great work. I did comment in his thread in the LM forum.

    There is still a lot of work left on this project and it won't be finished before 1. December though. I'll keep you updated.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  4. #4
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    84

    MorpHex, taking form

    Leg design

    To make MorpHex being able to curl up into a ball shape, I've decided to go for a little special leg design. Actually, MorpHex is a sort of dual hexapod, where one leg share a common coxa part with two femur and tibia parts.



    I'm using standard SES brackets, but pay attention to the ASB 15 v2 bracket that holds the two femur servos. The v2 bracket is just perfect for attaching the ASB-04 coxa bracket.



    5990's are used for the femur and 5645's for the tibia and coxa. Notice that the 5990 wires are guided through the 8 mm bearing/SES hole between the ASB-15 v2, LPA lexan spacer and the ASB-04 coxa bracket.


    Body modifications

    Since my first post about this project I've replaced the outer body parts from 1,5 mm to 2 mm thick aluminium, mainly for increased strength and stability (less flexing):



    Making sure that every gear is aligned correctly was the hardest part when assembling the body section. I solved it by carefully placing one gear at the time and mark the 4 SES holes on each outer bodysection, remove the section, drill the holes and mount the section onto the inner body section again. Repeated this process for all the 6 sections.



    Instead of using 3mm steel hex screws for holding the 12 ball-bearings onto the inner body I'm using 3mm threaded rods. The rods make it much easier for mounting a holder for battery and electronics.



    All the six legs are finally assembled, next step is to mount them to the body:




    MorpHex, taking form

    I know it looks kinda messy right now, but I do have plan, LOL. This picture show all legs mounted to the body and the upper part have their legs curled up into the ball shape position.



    Another picture illustrate MorpHex in the walk mode position:



    I've fixed some sphere parts with velcro just for giving you a little hint of how MorpHex are going to look like with all the sphere parts mounted:









    I might have to modify the feet a little bit (using smaller end caps and modify the ends of the tubes) so that they can be aligned even closer in the curled position. But these pictures illustrate how it's going to look like at the end:



    Just for visualization:



    This is one of my favorite pictures, it kinda remind me of the unfinished Death Star from Star Wars, LOL:

    Last edited by Zenta; 11-30-2010 at 05:55 AM.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  5. Re: MorpHex, a sphere formed morphing hexapod

    Wow. This is completely crazy.

    Very original ideas, and beautiful realization.

    At first I wondered where you would put that many servos in a hexapod, but now that I see it, I find this just brilliant.

    Consider my mind blown
    ---
    Personal blog: http://xevel.org
    USB2AX documentation: http://xevelabs.com

  6. #6

    Re: MorpHex, a sphere formed morphing hexapod

    Amazing

    You are an Artist.

    I cant wait to see the finished robot.

    Please keep posting picture.

  7. #7
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    84

    Re: MorpHex, a sphere formed morphing hexapod

    Thanks for your nice comment guys!

    Btw, for powering I'm planning two use this 2S LiPo battery I bought from Trossen Robotics. I really like the formfactor of this battery and they have a very good weight vs. capacity ratio.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  8. #8
    Join Date
    Oct 2008
    Location
    Calgary, Alberta Canada
    Posts
    95
    Rep Power
    48

    Re: MorpHex, a sphere formed morphing hexapod

    super creative dude! a+

  9. Re: MorpHex, a sphere formed morphing hexapod

    this is sick!

    have you put any thought into how you can make it roll in a controlled way? this has a very destroyer droid feel to it!

  10. #10
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    84

    Re: MorpHex, a sphere formed morphing hexapod

    Quote Originally Posted by kensbey View Post
    this is sick!

    have you put any thought into how you can make it roll in a controlled way? this has a very destroyer droid feel to it!
    Hi, Yes I've done many thoughts of how to control and interact with it. Also planning to add an 6 DOF IMU so that it always know how it's oriented.

    BTW:
    Sadly (or luckily) I won't be able to do much more about this project until next year because I got my #3 son last sunday night . So I'm a bit occupied with family and Christmas stuff at the time..
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Sphere Morphing Hexapod
    By innerbreed in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 11-03-2010, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •