Results 1 to 4 of 4

Thread: Whiteboard Erasing Robot

  1. Whiteboard Erasing Robot

    My entry for the TRC contest is a whiteboard cleaning robot. The goal of this project was to create a robot which could erase written text on a whiteboard completely autonomously i.e. no human interface. The processes involved in this project included devising a method for the robot to search a whiteboard for text, designing a way to physically move a robot to the text, and enabling a robot to erase the text.




    Parts Included:
    Arduino Mega
    Arduino Mega Protoshield, with 2 mini breadboards and jumpers
    3 VEX motors
    BlueSmirf Bluetooth Adapter (located in the yellow VEX case with antenna)
    RoboRealm Vision Software
    VEX linear sliders
    VEX Rack and Pinion gears
    VEX 9.6V Battery
    4 VEX small wheels
    Vex metal, screws, etc.

    This project is made up of two main sections. The first section is the actual robot. The robot in theory is somewhat simple. It consists of a base with two wheels which rides on a whiteboard track. The base design allows the robot to cover the entire x-axis of the whiteboard. To move on the y-axis, the robot uses linear sliders to move an arm up and down. Attached to the end of the arm is a dry-eraser that does the actual erasing.



    The second section, and more complicated part of the project, is the webcam and computer base control station located opposite the whiteboard. Utilizing an HD webcam and vision software at the computer base station, the robot locates any text anywhere on the whiteboard. It does this by using a series of filters and processing functions within the vision software, RoboRealm. In RoboRealm I used many different filters to find the center-of-gravity of the text on the whiteboard. The center of gravity cannot be found based on just the webcam image. I first used a RGB filter to eliminate everything but the green writing. Then the color is inverted by a Negative filter. The image is then converted from the Negative image ( the pink “hello”) to black and white using a gray-scale filter. This is necessary because the center of gravity can only be found on a black and white image. Then a center-of-gravity module is used to find the center of gravity. RoboRealm is a great software that has many uses and features. To find out more about the software go to www.RoboRealm.com











    Once the program finds the center of gravity of the writing on the whiteboard, it is converted to a point on a coordinate plane. Then using basic math, the program tells the robot to move to this point using motor commands derived from the point on the coordinate plane. All of the math and calculations are performed on the computer and only the motor commands are sent to the robot via Bluetooth. Performing the math on the computer and not on the actual robot makes the system perform significantly faster and smoother.







    One of the original goals of this project was versatility. This robot is designed to work on any whiteboard at my high school. Every whiteboard in the school has a track at the bottom for holding markers and erasers. By designing the robot to ride on this track, it can work anywhere in the school.



    However riding on this track proved a bigger challenge than I originally anticipated. The track at the bottom of the whiteboard is very narrow. In order to get the robot to stay on this track, I had to build the center of gravity directly over the track; otherwise it would fall off (which happened very frequently in the early design stages). This gave me a very small area to work in and I had to fit all the heavy parts into a tight area, hence the very messy and awkward placement of the battery and microcontroller.
    This project is a prototype that was a success and could be expanded greatly. There are many features that could be added to customize the robot in the future, such as

    • Automatic schedule, for example: erase every 10 minutes
    • Work with voice command instead of a webcam
    • A light sensor which would trigger the robot to erase the entire whiteboard when the lights go off i.e. when the teacher leaves the class room for the night
    • Only erasing certain color writing. Since the program uses a RGB filter, the robot could theoretically erase only red, green, blue, yellow, or cyan colored writing

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    127

    Re: Whiteboard Erasing Robot

    Very cool. Got a video of it in action?

    -Fergs

  3. Re: Whiteboard Erasing Robot

    Quote Originally Posted by lnxfergy View Post
    Very cool. Got a video of it in action?

    -Fergs

    Unfortunately I was not able to get a video of this robot in action. However I do have more photos of the inner workings of the robot if you would like to see them.

    Thanks,

    Ben

  4. Re: Whiteboard Erasing Robot

    Quote Originally Posted by 12grahamb View Post
    Unfortunately I was not able to get a video of this robot in action. However I do have more photos of the inner workings of the robot if you would like to see them.

    Thanks,

    Ben
    Nice project here. Can u send me the photos like what u said above,the working parts,tq

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry MARC: Military Armed Reconaissance Combat Robot
    By italian_guy299 in forum Project Showcase
    Replies: 3
    Last Post: 07-17-2011, 11:51 AM
  2. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  3. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  4. Project New Post For Fresh Start On Robot Butler
    By ROBOTMAN in forum Project Showcase
    Replies: 11
    Last Post: 10-31-2009, 12:50 PM
  5. Contest Entry Butler Robot
    By airman00 in forum Project Showcase
    Replies: 11
    Last Post: 07-31-2008, 09:28 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •