Results 1 to 4 of 4

Thread: Pi Robot gets inspired by Maxwell

  1. #1
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    49

    Pi Robot gets inspired by Maxwell

    [I just posted this to my little Pi Robot mailing list and thought I'd throw it up here too.]


    One of the benefits of being a robot is that you can swap out your parts more-or-less at will when new gadgets appear on the market. So when the $149 Kinect camera was released for the XBox game console, the robotics community took about a week to figure out how to use the camera to give their robots 3D vision. Pi Robot has actually had a Kinect since just before Christmas (no, he couldn't wait), but today he finally got to try it on.

    What you are about to see may shock you at first--Pi's familiar face has been transformed by the new technology. But as we will see, it is all for the best. Though bigger and heavier than a typical webcam, the Kinect provides both a regular color video image as well as a depth measurement at each point. It does this by projecting a pattern of structured infrared light out onto the world and uses a second camera tuned to infrared wavelengths to measure the distortion of this pattern caused by the shapes of objects in the scene. The result is a full depth map of every pixel in the image and at 30 frames per second.

    This first image shows Pi with his new head on.





    The Kinect camera is the black horizontal device at the top. It is wide because it has to accommodate two cameras and one projector. It also has two microphones, one at either end, that can be used to locate sounds. The tufts on top of the Kinect came as a little surprise, first discovered by Mike Ferguson (a.k.a "Fergs") at the University of Albany when he built his latest creation Maxwell shown here:





    So what do the 3-dimensional images look like? ROS includes a visualization tool called RViz which allows us to see both the regular video image and the 3D map from the Kinect. The 3D map can be shown in one of three ways: as the original RGB colors overlayed on the depth measurements; as a flat-color (e.g. gray) image; or as a color-coded image with red indicating objects closer to the camera and blue/violet labeling far away points. Here's what they look like:

    RGB Mode:




    Flat Gray Mode:



    Colorized Depth Mode ("Axis"):



    The last image perhaps best illustrates the quality of the depth map returned by the Kinect, with subtle changes in hue reflecting the distance of that point in the scene from the camera. Over the next several weeks and months, Pi will use this new 3D vision ability to begin recognizing real-world objects by size and shape, much as we do. Stay tuned!


    --patrick
    The Pi Robot Project
    http://www.pirobot.org

  2. Re: Pi Robot gets inspired by Maxwell

    Nice upgrade!

  3. #3
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    126

    Re: Pi Robot gets inspired by Maxwell

    We need to get a side-by-side picture of Maxwell and Pi at Robogames....

    -Fergs

  4. #4
    Join Date
    Apr 2009
    Location
    Stanford, CA USA
    Posts
    590
    Rep Power
    49

    Re: Pi Robot gets inspired by Maxwell

    Cheese!
    The Pi Robot Project
    http://www.pirobot.org

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry MARC: Military Armed Reconaissance Combat Robot
    By italian_guy299 in forum Project Showcase
    Replies: 3
    Last Post: 07-17-2011, 12:51 PM
  2. Contest Entry Whiteboard Erasing Robot
    By 12grahamb in forum Project Showcase
    Replies: 3
    Last Post: 03-01-2011, 07:51 AM
  3. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 10:20 AM
  4. Contest Entry The Pi Robot Project
    By Pi Robot in forum Project Showcase
    Replies: 18
    Last Post: 01-24-2011, 10:19 AM
  5. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-25-2010, 12:51 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •