Results 1 to 3 of 3

Thread: 3D Printer

Hybrid View

Previous Post Previous Post   Next Post Next Post
  1. 3D Printer

    I found this last night and I thought it was just amazing so I figured I would pass it on here. I'm highly impressed with its precision. Looks like this guy wants to open source his project some how. This is the guys blog. http://3dhomemade.blogspot.com/

    This is the 3D printer in action.

    Last edited by Robonaut; 05-24-2011 at 04:44 PM.

  2. #2
    Join Date
    Apr 2011
    Location
    Monterey CA
    Posts
    26
    Images
    15
    Rep Power
    28

    Re: 3D Printer

    Very nice resolution, he wants to make money. But does not seem to be greedy. 90% open source. sell10% in a kit. He would like to patent.
    jhertzberg

  3. Re: 3D Printer

    I too like the 90% open source deal. Depending on what to 10% kit looks like it could be a fairly attracting deal for me.

    I also like that Junior (the developer) talks about building a support community which I think is a great idea, I can only imagine that to be a lot of work. I hope it all works out well for him. I would really like to have one of these printers more than a makerbot or a reprap because of the resolution it offers.

    There also seems to be far fewer parts to deal with which makes me think the kit would be easier to build and maintain. My only true concern would be handling the resin and the fumes it gives off. I do have a good ventilation system in my shop which I'm sure would handle it fine. Just the same I think I will do more research on the resins toxic properties.

    If not for the current projects I have going on now I would attempt to make this on my own. From what I have read on some yahoo groups I seem to have all the components needed to make it. What I don't have is the program to run it all and the time for the trial and errors. So I think I will wait a bit to see how Junior makes out and what he ends up offering. He seems to be having a lot of success with what he has done already.

    Dang I really want one.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Interesting 3d Content Central
    By Quantum in forum Mechanics / Construction
    Replies: 3
    Last Post: 09-24-2011, 12:55 AM
  2. 3D Head Tracking Tutorial - Part 1
    By Pi Robot in forum ROS - Robot Operating System
    Replies: 9
    Last Post: 03-19-2011, 08:37 AM
  3. Google SketchUp to 3D printing?
    By Pi Robot in forum Mechanics / Construction
    Replies: 5
    Last Post: 03-02-2011, 10:25 AM
  4. Considering adding humanoids to our 3D simulator (Cogmation's robotSuite)
    By HumanoidFan in forum Software and Programming
    Replies: 2
    Last Post: 03-29-2008, 02:47 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •