Results 1 to 8 of 8

Thread: Want to build a backhoe or a crane ARM

  1. Talking Want to build a backhoe or a crane ARM

    I would like to build a backhoe robot arm. It could also be something like a crane, where it's not just a bucket at the end, but more like a claw, or a hand.

    I have a question as to what parts I should use for the "joints." I have started down the path of using motors, with phidget motorControl boards, but I am realizing that I may want to use servos instead.

    The goal is to have a robotic arm that can play and dig in a sandbox. If you can picture that.

    Has anyone built something similiar? Do you have a link to something similar? Do you have suggestions on parts, like should I use servos, or can I get by with motors?

    Thanks in advance for your input!
    The Space Cowboy
    -= Its all about cams and kars =-
    http://www.mycamcar.com

  2. #2
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    97

    Re: Want to build a backhoe or a crane ARM

    So a couple of questions before I think we can give you much help. Servos is probably the route you will end up going, but I am concerned that you are going to be pretty disappointed. The problem is, most of the hobby scale robot arms (kits and scratch built) don't have a very high payload capacity so if you want to "play in the sand" with it, you are looking at playing on a very small scale unless you want to build a very expensive arm.

    You could go with linear servos which would increase your payload by a lot, but would also come at a cost of about $145 per joint by the time your done, which all said and done may end up on the relative low end...

    I would also think you will need to be careful not to have sand bunging everything up.

    Hope this helps

    DB
    http://forums.trossenrobotics.com/tu...searchid=16136

  3. Re: Want to build a backhoe or a crane ARM

    here's a pic of one i made (http://forums.trossenrobotics.com/sh...highlight=quad) it took five Dynamixel AX-12A's and it worked great adn it was just attached with a few of the regular bioloid frame parts

  4. Re: Want to build a backhoe or a crane ARM

    Hey darkback2, thanks for the link you sent. Looks very helpful to examine the mechanics of the arm.

    I'm going to go through this and see what I come up with. My first stab is going to be with a motor / winch type of system and see how that pans out. It also seems that most backhoes in real live use some sort of pole-type actuator, where it extends and retracts.

    Good point about the sand too. I will have to think about that.
    -= Its all about cams and kars =-
    http://www.mycamcar.com

  5. Re: Want to build a backhoe or a crane ARM

    Real life backhoes use rams with hydrolics.

    Kar

  6. Re: Want to build a backhoe or a crane ARM

    "Rams." Yea, I guess that's what you would call it. A "ram actuator." Perhaps that is the right way to go long term. Where can I get one of these types of actuators?
    -= Its all about cams and kars =-
    http://www.mycamcar.com

  7. #7
    Join Date
    Jan 2010
    Location
    Texas
    Posts
    58
    Images
    7
    Rep Power
    34

    Re: Want to build a backhoe or a crane ARM

    I have seen some amazing creations with motors. Do a little digging into the meccano shows and see some of the scale replicas they bring to life via motors and metal gears as well as pulley systems. Ive often added phidgets into meccano projects to control motion. I would think with motors you may want to utilize a few pots for positional report back to the program. As for framework i would suggest aluminum over the plastic bioloid pieces for digging in the sand. The metal will give a more authentic look also.

    Just my 2 cents, might not be worth that ... lol

    Meccano Jay ...
    find me @ http://www.phidgets.com/phorum as well and Happy Building!!



  8. #8
    Join Date
    Jan 2010
    Location
    Texas
    Posts
    58
    Images
    7
    Rep Power
    34

    Re: Want to build a backhoe or a crane ARM


    Meccano Jay ...
    find me @ http://www.phidgets.com/phorum as well and Happy Building!!



Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Experience with ROS Arm Navigation and Grasping?
    By Pi Robot in forum ROS - Robot Operating System
    Replies: 12
    Last Post: 02-02-2011, 08:25 AM
  2. Selecting Components for DIY Robotic Arm
    By tikka308 in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 07-05-2010, 08:53 PM
  3. Xan's Rover with Arm
    By Xan in forum Rovers
    Replies: 14
    Last Post: 07-18-2009, 01:16 AM
  4. Project Custom joystick to control robot arm
    By HakBot in forum Project Showcase
    Replies: 22
    Last Post: 08-22-2008, 10:44 AM
  5. Replies: 30
    Last Post: 05-29-2008, 10:47 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •