Hi everyone. After converting my 22 DoF AX-12 hex to a biped, I have come up against the old "Ankle servos getting too hot" problem. I have worked out a simple hinge & lever design that would reduce my available foot tilt to + or - 20 degrees & increase the holding torque significantly, but that leaves the lever only connected to the servo-horn by one 2mm bolt. Basically, the servo pushes a hinged lever down (23mm centre to centre), which is connected to the foot, while the foot tilts on a hinge set 16mm off to one side, & approx 23mm below the centre of the servo-horn.
Apart from the increased 'slop' due to the tolerances in the lever & hinge connections, is there any point to me bothering to make it? I.E. Have any of you done this already & found the problems?
I have access to a lathe, so if the connection to the servo horn needs strengthening, then I should be able to make up a little plate to allow all four servo-horn bolts to be used, with the lever bolting seperately to the plate, but I guess my question is more about the basic mechanics of the system - Will it, or 'should it' work? - I am trying to play "Devils advocate" to make sure I have covered all potential issues.
The reduced range of movement should be more than sufficient for walking on flat ground, while the available 20kg/cm holding torque when the foot is level, & much higher when the foot is at 20 degrees tilt, should prevent the servo overheating. Disclaimer - My torque calc's may be wrong! The foot doesn't need to be tilted fast, so lack of speed shouldn't be an issue either, & it doesn't make it that much taller compared to the normal plastic brackets. The extra weight will be low down, & will only be a few grams.
PS DarkBack - Yes, I know that it really means that my robot is too fat.........I WANT to carry more uneccessary weight, while being able to maintain static stability in the entire stepping motion. I hate shuffling, so replacing the servo with a hinge & two opposing springs is not my preferred option.
Bookmarks