Results 1 to 3 of 3

Thread: 6dof Stewart platform hexapod

  1. #1

    6dof Stewart platform hexapod

    Well this project is exactly what it says it is...

    This is a 6dof Stewart platform hexapod.
    A Stewart platform is a type of parallel robot that incorporates six servos arranged in a prismatic layout.
    The servos are mounted in pairs to the base, crossing over to three mounting points on a top (Target) plate.
    Devices placed on the Target plate can be moved in the six degrees of freedom in which it is possible for a freely-suspended body to move.






    These are the three linear movements x, y, z (lateral, longitudinal and vertical), and the three rotations pitch, roll, & yaw.

    Now the interesting part.. :lol:


    Does anyone have experience with a Stewart Platform, running on the Basic Atom Pro28?

    anyway there it is, i hope its of interest?!
    -------------------
    LYNXMOTION on FACEBOOK!

    Jonny Poole,
    IΠΠΣΓBΓΣΣD.

  2. #2
    Join Date
    Jun 2010
    Location
    Australia
    Posts
    161
    Rep Power
    28

    Re: 6dof Stewart platform hexapod

    Sorry, no experience here, but looking from the outside, if each right hand servo in each pair moved up, & each left hand one moved down, would the target plate / head rotate clockwise? Looks like you can get limited rotation as well - Plus or minus 30-40 degrees or so depending on the ball joints. Chuck a dolls head on it & you could get some freaky animatronic head movment going!

  3. Re: 6dof Stewart platform hexapod

    It looks good, but as far as I know it's not exactly a Stewart platform.
    These things are normally done using linear actuators. Using rotating actuators the way you do will have a direct impact on the kinematics of the system, and you won't be able to use equations from a canonical steward platform.
    (And btw, I studiet Steward platforms at school, deriving their equations is not exactly funny...)

    Do you want to control it using IK ?
    Last edited by Xevel; 07-19-2011 at 08:42 PM.
    ---
    Personal blog: http://xevel.org
    USB2AX documentation: http://xevelabs.com

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Cad Design for Hexapod
    By epsilonorion in forum Robotics General Discussion
    Replies: 1
    Last Post: 10-03-2010, 07:17 PM
  2. Project Scuttle - 4DOF Hexapod
    By blobbington in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 08-16-2010, 02:24 PM
  3. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-25-2010, 12:51 AM
  4. News/Announcement micromagic hexapod kit MSR-H01
    By mdenton in forum Humanoids, Walkers & Crawlers
    Replies: 33
    Last Post: 10-04-2008, 06:37 AM
  5. Hexapod using 60mm (1/5 scale) Servos
    By mdenton in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 05-06-2008, 02:51 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •