PART 1
I've been trying for a while to use the ZIG2Serial I just bought, but for a unknown reason, it doesn't work.
I've done what is written on http://support.robotis.com/en/ under: Product Information > Robot Parts > Communication > ZIG-100/110; but I still get this Error:
First: I think my computer is supposed to provided the power, and the light on the Zig2Serial is open which confirmed that it receives current.Unable to find Zig2Serial. Please check the following and try again.
-Is power being supplied to the Zig2Serial?
-Is the Zig2Serial connected to the proper port?
Second: Yes, and Ive try all ports just in case.
The Zig100 is connected to the Zig2Serial and the Zig110 is connected CM-510.
And when I do this: "While pressing on “1” (Shift+1) on your keyboard also press the reset switch on the Zig2Serial." in the RoboPlus terminal software, it doesn't work neither.
Does someone have an idea what is going wrong?
PART 2
Can I use Matlab with the Zig2Serial? Because it doesn't seem to be in the options on the web site under: Software Help > Zigbee SDK > Zig2Serial > Windows
Any help would be very appreciated, thanks.
Bookmarks