Results 1 to 10 of 10

Thread: Quad balance

  1. Quad balance

    I have recently built a quad and I've figured out how to make it walk but it becomes unbalanced when it lifts up one of the legs and I was wondering how to fix that

  2. #2
    Join Date
    Jun 2011
    Location
    USA
    Posts
    542
    Images
    107
    Rep Power
    41

    Re: Quad balance

    Quote Originally Posted by blastdog View Post
    I have recently built a quad and I've figured out how to make it walk but it becomes unbalanced when it lifts up one of the legs and I was wondering how to fix that
    Do you have pictures? In general, you need to keep the center of mass in mind... namely the other three legs form a triangle on the ground. The center of mass needs to be within that triangle for static stability.

  3. Re: Quad balance

    here are some pictures any suggestions?

  4. #4
    Join Date
    Jun 2011
    Location
    USA
    Posts
    542
    Images
    107
    Rep Power
    41

    Re: Quad balance

    Since you're using wheels, you're essentially standing on 4 points, at most. With other quads, the feet have width so that there are multiple points of contact on the ground, and thus stability. What you could do is put 3 wheels on each foot and have the two outer ones be free-spinning, and unpowered. They could be ever so slightly smaller diameter than the center wheel too. Just an idea....

    It sounds like you're starting with 1 leg off the ground at a time... This graphic for a walk with 2 legs off the ground at a time sort of illustrates the center of mass problem (note the intersection of red lines moves...)

  5. #5
    Join Date
    Sep 2010
    Posts
    205
    Images
    16
    Rep Power
    38

    Re: Quad balance

    Wider feet help because you get more then one contact point with the ground per foot. This does cause 'scrubbing" when the feet rotate though. Depending on the surface you are walking on, this may or may not be an issue.

    If you want feet to be more like a point contact, you can program the center of mass of the robot to always be between the 3 legs contacting the ground. This is a common way to do it when using a ripple gait. But you need to be aware of the dynamic forces involved, if you lift one leg up quickly it will make the robot tend to fall. If you use a amble gait (2 legs moving at a time) you can somewhat balance this movement.

    Another thing you can do is make the feet lift and return to the grounnd quick enough that it doesnt have time to fall over, the bot will rock a bit though.

  6. Re: Quad balance

    Thanks for the advice and it will have treads on the wheels too

  7. #7
    Join Date
    Jun 2011
    Location
    USA
    Posts
    542
    Images
    107
    Rep Power
    41

    Re: Quad balance

    Quote Originally Posted by blastdog View Post
    Thanks for the advice and it will have treads on the wheels too
    It's a general concept to play around with and find what works well

  8. Re: Quad balance

    Thank you sooooooo much I've fixed the wheels and made them a lot thicker and now it balances great

  9. #9
    Join Date
    Jun 2011
    Location
    USA
    Posts
    542
    Images
    107
    Rep Power
    41

    Re: Quad balance

    Quote Originally Posted by blastdog View Post
    Thank you sooooooo much I've fixed the wheels and made them a lot thicker and now it balances great
    Awesome Now post more pics ;D

  10. Re: Quad balance

    Will do I have a video of it walking that I'll post when I get around to it all I need to do is write the actual program and adjust some timing things

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. My 4DoF Quad Mech: Numa
    By Gertlex in forum Mech Warfare
    Replies: 41
    Last Post: 08-12-2012, 11:58 PM
  2. Project Draco 08 - Quad Mech
    By elaughlin in forum Project Showcase
    Replies: 148
    Last Post: 04-12-2011, 07:09 AM
  3. Rover, 'pod or quad?
    By Stobs in forum Mech Warfare
    Replies: 25
    Last Post: 11-08-2010, 01:29 PM
  4. Contest Entry Mammalian Inspired Quad IRON WOLF
    By innerbreed in forum Project Showcase
    Replies: 2
    Last Post: 09-04-2010, 11:27 AM
  5. Project Felix, a SES based 4x4 DOF quad
    By Zenta in forum Humanoids, Walkers & Crawlers
    Replies: 35
    Last Post: 08-01-2009, 01:45 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •