Results 1 to 2 of 2

Thread: (Questions) How to use USB2Dynamixel under 64v bit Ubuntu 12.04

  1. (Questions) How to use USB2Dynamixel under 64v bit Ubuntu 12.04

    Dear All.
    I want to know how to use this device under ubuntu 12.04. Since there is no *.c or *.h in /usb/serial directory. So I cannot follow the steps following website.
    http://support.robotis.com/en/softwa...2dxl_linux.htm

    Who can tell me how to use it ,since now I can not use it, when I try the demo example, it told me it can not find tty/usb0. Though I can use lsusb find it, and use sudo chmod 777 /dev/bus/usb/002/00* to make it can R/W.
    Thanks for any help.
    Zhenli

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: (Questions) How to use USB2Dynamixel under 64v bit Ubuntu 12.04

    You do not need to compile drivers for the USB2Dynamixel. Read the instructions I left in the other thread you posted in. The USB2Dynamixel will be identified to the system as "/dev/ttyUSB#", where # is some number (usually 0, unless you have multiple USBtoUART devices connected).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) USB2Dynamixel in Ubuntu Natty
    By Chmaanta in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 02-01-2013, 03:28 PM
  2. Dynamixel RX-24F and RS-485 Communication on Linux/Ubuntu
    By robot in forum Software and Programming
    Replies: 2
    Last Post: 09-06-2012, 04:25 AM
  3. Starting with ROS/Ubuntu - Installing a package
    By Martijn in forum ROS - Robot Operating System
    Replies: 4
    Last Post: 08-01-2011, 03:12 PM
  4. Roboard ubuntu installation problem
    By moogly in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 04-17-2011, 07:19 AM
  5. Question(s) FTDI USB Breakout driver on Ubuntu
    By zzl1007 in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 11-19-2010, 02:39 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •