Results 1 to 3 of 3

Thread: Modding battery wire?

  1. Modding battery wire?

    I have a 6v 2300mAh NIMH battery with a crappy small wire attached to it (maybe can handle 2 amps)
    My robot legs' max amp draw would be 8 amps @ 5v (about 30 min runtime)
    However since the battery wire is so small it can't deliver the 8 amps.
    Is it safe for me to cut it open and switch in a beefier wire?

    How do you guys deal with the amps your robot consumes?

  2. #2
    Join Date
    Dec 2008
    Location
    Washington
    Posts
    312
    Images
    35
    Rep Power
    41

    Re: Modding battery wire?

    Do you know the gauge of the wire that came with the battery? Unless you feel the wire overheating you might not need to switch it out, but if it dose overheat you could open up the battery and replace all crappy wire as long as your comfortable doing it. There shouldn't be any issues as long as you do it right
    Dalton Caughell

  3. Re: Modding battery wire?

    While this is doable, you have to be careful not to damage the cells. If they get too hot during soldering they are very easy to damage. If the battery has tabs, soldering to those greatly alleviates this =)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Modding a Toyeast/Mato Toys tank gun
    By mannyr7 in forum Mech Warfare
    Replies: 3
    Last Post: 02-28-2011, 01:39 PM
  2. Dynamixel connector wire
    By Adam in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 06-02-2010, 11:48 AM
  3. Replies: 23
    Last Post: 05-13-2010, 08:15 PM
  4. Where does everyone buy bulk wire?
    By Sienna in forum Mechanics / Construction
    Replies: 5
    Last Post: 07-02-2009, 11:41 PM
  5. Servo Wire Length
    By pottsbgstv in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 08-01-2007, 04:59 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •