Results 1 to 2 of 2

Thread: PC based robot

  1. #1
    merogg Guest

    PC based robot

    Hello!

    Found this nice forum when browsing for information. Anyway, I'm planning to build a PC based robot with a mini ITX board, but I'm stuck on a few questions.

    What's the average power consumption of a mini ITX board? I could not find it anywhere in the manufacturer's specifications. Let's say my processor uses max 35W. Will a 80W picoPSU be able to power the system if there won't be anything else other than CPU, HDD and a fan connected to my motherboard?

    Also, since picoPSU's input is unregulated, is it safe to plug it directly to a LiPo battery (the motherboard will get 11.1 to 12.6 V).


    Thanks

  2. Re: PC based robot

    Which ITX boards are you looking at ? Any particular software that needs an Intel CPU underneath ?

    If not, and you are concerned about power usage, i'd actually recommend looking at ARM based solutions, like OMAP with BeagleBoard or the more powerful dual-core Cortex-A9 http://pandaboard.org/

    If you are running Linux on it anyway, it should not make much difference from software perspective.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Another Scout Based Robot
    By Firestorm65 in forum Mech Warfare
    Replies: 43
    Last Post: 04-17-2009, 07:59 AM
  2. PC based robot frames
    By asbrandsson in forum Mechanics / Construction
    Replies: 47
    Last Post: 11-13-2008, 09:39 AM
  3. Question(s) Stream webcam from PC based robot
    By anandoc in forum Sensors
    Replies: 9
    Last Post: 11-07-2008, 06:07 PM
  4. Creating a PC-based Mobile-Robot with Arm
    By wmccafferty in forum Robotics General Discussion
    Replies: 29
    Last Post: 01-17-2008, 04:05 PM
  5. PC-based robot help
    By Mr-Olsson in forum Robotics General Discussion
    Replies: 8
    Last Post: 09-14-2007, 03:47 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •