Page 5 of 5 FirstFirst 12345
Results 41 to 44 of 44

Thread: Some XV-11 notes

  1. Re: Some XV-11 notes

    Quote Originally Posted by jetdillo View Post
    ...the top hits are still some of your older pages, ...
    Not mine, Hash's. He made a looot more stuf about the LIDAR than I did

    I am really disappointed that the XV-11 only found its way in very few robots. It has so much potential! The kinect got to be used by everyone and their dogs, while I can probably count the robots with a Piccolo Lidar on the fingers of my hands :/
    I guess what it needs is more publicity ^^
    ---
    Personal blog: http://xevel.org
    USB2AX documentation: http://xevelabs.com

  2. #42
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    285

    Re: Some XV-11 notes

    If one could buy the LIDAR as a spare part, I would buy one in a heartbeat. Though, as it stands, $400 is still just a bit too much for me to spend on a nice and very inexpensive LIDAR unit attached to a robot that I will likely never use.
    Last edited by tician; 11-03-2012 at 10:15 PM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #43
    Join Date
    Nov 2010
    Location
    Fresno,CA
    Posts
    170
    Rep Power
    41

    Re: Some XV-11 notes

    Speaking of updating material I got one that should help out quite a bit! The new 2.6 firmware removed the " help" hidden help command that listed all the extra menu items. You can get back all the menu items and the " help" command if you simply press and hold the orange Start button and the Back button (curly arrow) at the same time for ~4 seconds.

    If you want to read more about it check out my blog post with data dumps from the on-board 4 pin UART showing the different boot mode.

    http://random-workshop.blogspot.com/...-firmware.html

    -Hash

  4. Re: Some XV-11 notes

    Why don't you look on Ebay? I bought three slightly used for less than $200.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •