Page 4 of 7 FirstFirst 1234567 LastLast
Results 31 to 40 of 66

Thread: USB2AX v3.0a feedback

  1. #31
    Join Date
    Sep 2008
    Location
    Toronto, Ontario
    Posts
    171
    Images
    43
    Rep Power
    40

    Re: USB2AX v3.0a feedback

    Thanks tician!


  2. #32

    Re: USB2AX v3.0a feedback

    Quote Originally Posted by KevinO View Post
    Are these still for sale? I'm using the usb2dynamixel but this would be a dream to use instead due to it's size.
    Is it the same as the ones at seeedstudio?
    http://www.seeedstudio.com/depot/usb2ax-p-1349.html

    Kurt

  3. #33
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: USB2AX v3.0a feedback

    Quote Originally Posted by KurtEck View Post
    Is it the same as the ones at seeedstudio?
    http://www.seeedstudio.com/depot/usb2ax-p-1349.html

    Kurt
    Pretty sure that it is, just with the new OpenHardware logo silkscreen (and likely professionally manufactured) instead of the wavy deal (and hand-assembled by xevel). The link at the seeedstudio shop goes to xevel's USB2AX dev site and it lists him as the designer.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  4. Re: USB2AX v3.0a feedback

    Yes it is. I have to apologize for the way this has been developping during these last month. The first batch has been finished around the beginning of the year, but I was very busy with two trips to India and a whole lot of life changes, so much that I set aside the USB2AX for around two months...
    The quality of the boards assembled by Seeed (or more precisely by their contractors) is completely satisfactory, even the shrink wrap is perfectly as I wanted it I have tested a few and it's exactly as expected.

    The USB2AX sold on Seeedstudio is indeed mine, I did not do any advertisement about it on purpose: the documentation is not online, and I did not want to deal with lousy support- no time to do it properly...
    Just for your information: each unit producted is tested before being considered valid. I paid for 200 units, they made 205, had 12 ones not passing the tests the first time, and only two could not be fixed - according to the test report.

    Things are looking better though, but I'm not doing any more promises on dates, for I have disappointed everyone who might have taken my previous ones seriously.
    For those interested, they might be sold on the Trossen Robotics store soon.
    ---
    Personal blog: http://xevel.org
    USB2AX documentation: http://xevelabs.com

  5. #35
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    43

    Re: USB2AX v3.0a feedback

    Got my USB2AX working with Windows 8 (my shiny new Surface Pro) as well. In this case, it complains about using an unsigned driver (same file as I mentioned on previous page). The solution to this is to google the error message; there are lots of guides/vids for getting around this issue. It's not hard to do, but worth noting in user-guides.

  6. Re: USB2AX v3.0a feedback

    Ok, thanks! I'll make sure to put it somewhere for all to see
    ---
    Personal blog: http://xevel.org
    USB2AX documentation: http://xevelabs.com

  7. #37

    Re: USB2AX v3.0a feedback

    Great! I will buy one! And any shop around Europe?

  8. Re: USB2AX v3.0a feedback



    No shop in Europe right now but it might change soon, next week will be determinant in that regard.
    In the meantime I can sell you some myself (I'm in France), the ones I have here are from the same batch so it won't be a prototype
    Send me a MP if you are in a hurry.
    ---
    Personal blog: http://xevel.org
    USB2AX documentation: http://xevelabs.com

  9. #39

    Re: USB2AX v3.0a feedback

    Ok, thanks

  10. #40

    Re: USB2AX v3.0a feedback

    Click image for larger version. 

Name:	20130321_150227761538286.jpg 
Views:	231 
Size:	60.8 KB 
ID:	4592Click image for larger version. 

Name:	USB2AXoverUSB2Dynamixel.jpg 
Views:	240 
Size:	129.0 KB 
ID:	4594

    I just received it. It's really tiny! I (will upload) have uploaded a new photo next to a USB2Dynamixel from Robotis.

    And it's faster, some first tests:
    (querying 16 AX-12)
    Poll test, conn USB, duration 00:00:00.2500000 COM3 USB2Dynamixel

    Poll test, conn USB, duration 00:00:00.0625000 COM7 USB2AX

    You should remember that in Linux it appears as ttyACM0, not TTyUSB0 as USB2Dynnamixel.

    Last edited by siempre.aprendiendo; 03-22-2013 at 04:26 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Regarding Dynamixel Positional Feedback Demo
    By DiegoSpinola in forum Robotics General Discussion
    Replies: 4
    Last Post: 12-06-2011, 05:09 PM
  2. Project Handmade 5DOF Manipulator with tactile feedback
    By Antonb in forum Project Showcase
    Replies: 9
    Last Post: 03-11-2011, 05:50 PM
  3. Question(s) Using AX-12's present-load feedback
    By RobotAtlas in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 07-04-2010, 08:33 PM
  4. Question(s) Pololu 3A Motor Controller with Feedback
    By kankatee in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 12-22-2008, 07:53 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •