Results 1 to 4 of 4

Thread: Reading Dynamixel's position in Wheel Mode

  1. Reading Dynamixel's position in Wheel Mode

    Hello,

    After some googling I still don't have a clear answer. It seems that higher end models (MX-28 and EX-106+) will return a valid position value (overflowing) in wheel mode. All other models have a dead zone and this caution note in their manuals: "If it is set to Wheel Mode, the value cannot be used to measure the moving distance and the rotation frequency".

    I'm most interested in AX-12A behavior. Can someone verify that they read valid position values in wheel mode (except when in dead zone) from AX-12A?

    Thank you,
    Paul
    Last edited by pauljurczak; 10-28-2011 at 06:35 AM.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,258
    Images
    27
    Rep Power
    273

    Re: Reading Dynamixel's position in Wheel Mode

    See here.

    The MX-28 has a single magnetic encoder that produces an absolute position for the entire 360 degrees of rotation, in both wheel and servo modes, with values from 0 to 4095.
    The EX-106+ has a rotary encoder for wheel mode that does not produce an absolute position value, only a relative value (a 16-bit counter that increments for CCW rotation and decrements for CW rotation with each count being ~0.06 degrees). It also has an absolute position sensor (standard potentiometer?) that only produces a valid value when in servo mode (with the same dead zone as all other non-MX series servos).
    The AX-12A, like all other dynamixels not described above, cannot produce a valid position value when in wheel mode (it is even stated in a big yellow box preceded by a graphic exclamation point).
    Last edited by tician; 10-28-2011 at 09:01 AM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  3. Re: Reading Dynamixel's position in Wheel Mode

    Thank you for clearing this up. BTW, the thread you linked to contains this from Robotis guy: "... the new MX-28 (and other MX series) ...". Do you have any information about other MX series?

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,258
    Images
    27
    Rep Power
    273

    Re: Reading Dynamixel's position in Wheel Mode

    No idea about anything yet, but it is not unexpected that they would shift more of their existing products to the newer controller/sensor boards. No more worn potentiometers (contactless magnetic encoder), higher dynamixel bus data rates (72MHz STM32 vs 16MHz of the ATmega8), and 32-bit math for position and speed control (32-bit ARM Cortex-M3 core versus 8-bit AVR core of the ATmega8).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Does Dynamixel servo AX-12 or RX-64 have motor lock mode?
    By bonmot in forum Humanoids, Walkers & Crawlers
    Replies: 6
    Last Post: 03-25-2011, 10:56 PM
  2. Wheel position sensor positioning
    By Resilient in forum Sensors
    Replies: 2
    Last Post: 03-14-2009, 01:34 AM
  3. Anyone got Sabertooth packetized mode to work?
    By shobley in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 01-25-2009, 08:28 PM
  4. Motor Mount & Wheel Kit with Position Controller
    By ctx32 in forum Robotics General Discussion
    Replies: 7
    Last Post: 08-01-2008, 08:42 PM
  5. Sabretooth 2x10 - in p-serial mode
    By shobley in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 02-15-2007, 04:21 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •