Results 1 to 7 of 7

Thread: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

  1. Thumbs up A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    Hey all, as promised here's a preview of my VIMPHIN - A Reconfigurable Virtual Manipulator Physical Interface
    which is meant to be an OpenSource haptics interfacing device for VR&AR (haptic feedback is coming soon to the next version):


    demo video:
    http://www.youtube.com/watch?v=WsTm8flq-lw


    It's for my masters degree project and as soon as v0.3b is out i'll release everything (FW/Assembly/InterfacingLibs/DemoApp) under an OSHW compatible license


    What do you guys think of it?

    Diego
    Last edited by DiegoSpinola; 12-03-2011 at 01:35 PM. Reason: adding a picture

  2. Re: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    VIMPHIN is back! now implementing haptic feedback! Collision with virtual objects and variable resistance to motion!
    checkout the videos below :




    and a bonus: Pointcloud generating 3d scanner =D

  3. Re: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    Thats really nice, i like how you keep adding new features, especially the pointcloud one is impressive. Apart from your thesis(?) are you thinking of making it a actual product? (like some advanced 3d mouse) or will it just be for you?

  4. Re: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    @Suicidal.Banana :
    Thanks! The Idea is to create a low cost "kit" that can be distributed among laboratories (or individual researchers/students) that are currently researching haptics =) (attempting to lower the entry cost on the field)



  5. Re: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    Nice idea!

    Also, i was wondering, did you try combine the two yet? it would be pretty freaky to have feedback when using it with the pen, "feeling" a 3d object on your screen.

  6. Re: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    I haven't tried to combine the two modes yet, I'll put it on the TODO list at the Lab

  7. Re: A Reconfigurable Virtual Manipulator Physical Interface (VIMPHIN)

    Hehe ok, good luck

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Maxwell: A Mobile Manipulator
    By lnxfergy in forum ROS - Robot Operating System
    Replies: 45
    Last Post: 12-28-2012, 09:36 PM
  2. Interesting RX-28M with TTL interface & 12V
    By RobotAtlas in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 05-16-2011, 12:22 PM
  3. Project Handmade 5DOF Manipulator with tactile feedback
    By Antonb in forum Project Showcase
    Replies: 9
    Last Post: 03-11-2011, 06:50 PM
  4. How can I programatically "press" a physical button?
    By nagmier in forum Robotics General Discussion
    Replies: 16
    Last Post: 09-08-2009, 01:06 AM
  5. Virtual Testing
    By Firestorm65 in forum Mech Warfare
    Replies: 5
    Last Post: 02-22-2009, 12:45 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •