Results 1 to 3 of 3

Thread: Two negatives, One positive?

  1. Question Two negatives, One positive?

    Hello, the major hardware builds on my robot are done, but there are somethings I'm not quite certain about; in particularly, the powering and grounding of my motor circuits.

    Basically, the motors themselves have a power source only they use, ( 4 C batteries.) the rest of the components on the bot are powered by a single 9 volt battery.

    Now, the instructions say to ground everything to pin 23 of the BS2, which is connected to the negative pole, including the motor circuits.

    So, the motor circuits are connected to the power and ground on the 4 C batteries, and to the ground on the 9 volt battery.

    My question is if I should connect the motor circuits to the power of the 9 volt battery as well.

  2. #2
    Join Date
    Jul 2008
    Location
    South Sphincter Idaho
    Posts
    613
    Images
    104
    Rep Power
    64

    Re: Two negatives, One positive?

    It's a good idea to always have all of the grounds connected together. It doesn't hurt anything, and can stop other problems from surfacing.

    Keep the positive feeds separated.

    Gary
    Team Maggot---Mechs. "Bheka" (retired), "Maggot Mk.3(A)"
    " Keep your stick on the ice ".... Red Green

  3. Re: Two negatives, One positive?

    ok, thank you.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •