I have a curtis 4015a lcd tv. Screen went out, I just fiqured it was going to be the typical capacitor blown. Well when opened I found the two high voltage leads were taped to the back of the screen. They then at that point got so hot that the wire coating cracked and shorted. There are ceramic capacitors at the ends of both. they are marked with a high voltage symbol on the circuit board. there are no markings on the capacitors. I don't know how to identify them for replacement. I'm pretty sure they or one have blown. one of them is discolored. Any help please. My Son the electronics guru says I can't fix it throw it away. I'm trying to prove the smart as- wrong.
Bookmarks