Re: Connectors and wire.
If you ever decide not to buy pre-assembled cables, then be warned that you also have to buy the wire, crimp pins, and a crimper to actually make a cable (although having exact/custom length cables can be nice). Finding high strand count, small diameter (thus flexible) wire can be a bit difficult and expensive. There have been others to use cheapo/generic VGA pin crimpers from radioshack to successfully crimp the pins for the molex connectors, but I went with a cheap-ish crimper specific to molex crimp pins. There is a bit more in this thread, but it is only relevant if you are making your own cables (and yes, I was able to crimp 20AWG wire with those pins and crimper).
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"I give you 80mg fluoxetine, 10mg buspirone (4x daily), plenty of food and sleep, and still you are failing me, Brain!"
Bookmarks