Trossen Distance Sensor  Top Banner
+ Reply to Thread
Results 1 to 2 of 2

Thread: Neato XV-11 charging base identification

  1. #1
    Join Date
    Nov 2010
    Location
    Sunnyvale, CA
    Posts
    55
    Rep Power
    9

    Neato XV-11 charging base identification

    The XV-11 charging base has a kind of "picket fence" bar code behind an IR-transparent window. It shows up on the LDS scan and that presumably is how the XV-11 does the "wiggle dance" to back into the charger when it docks. Has anybody here tried to do their own docking routine using that? Has anybody here put any time into analyzing the docking base signature in the LDS data? I've been thinking about how to do docking -- it seems like its a bit of a pattern recognition problem -- I'm not to up on pattern recognition, however...

    Ideas welcome.

    -dave

  2. Re: Neato XV-11 charging base identification

    Quote Originally Posted by DaveC View Post
    The XV-11 charging base has a kind of "picket fence" bar code behind an IR-transparent window. It shows up on the LDS scan and that presumably is how the XV-11 does the "wiggle dance" to back into the charger when it docks. Has anybody here tried to do their own docking routine using that? Has anybody here put any time into analyzing the docking base signature in the LDS data? I've been thinking about how to do docking -- it seems like its a bit of a pattern recognition problem -- I'm not to up on pattern recognition, however...
    I can see the pattern in the LDS data.. it is pretty obvious as wildly varying brightness values that match a pattern.. the bad part is that those values are very random depending on distance and angle and lighting and who knows what else.. One thing I know for sure is that the brightness data saturates completely if you are close to the dock and becomes unusable.

    Distance data is fairly reliable but brightness data is just a disaster.. I honestly don't see how to use such poor data to find the dock.. I wouldn't be surprised if the shape of the dock is a factor in the final docking maneuver because shapes are so much easier for the XV-11 to see and consistent to the end

    If I wanted to make an XV-11 dock I would build a dock with a unique shape that was easy to track.. maybe something just like the bar code only using varying distances.

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. NiMH charging oddity
    By n5296s in forum Power
    Replies: 2
    Last Post: 07-05-2010, 07:51 PM
  2. Bioloid CM-5 not charging
    By vafvaf in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 02-17-2010, 11:53 AM
  3. Charging batteries
    By shobley in forum Mechanics / Construction
    Replies: 11
    Last Post: 06-28-2009, 03:22 PM
  4. open source sound identification and location
    By Resilient in forum Software and Programming
    Replies: 4
    Last Post: 04-16-2009, 11:31 PM
  5. charging and battery system
    By asbrandsson in forum Brains of my Robot
    Replies: 1
    Last Post: 01-29-2008, 04:54 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts