Results 1 to 9 of 9

Thread: Arbotix, Arduino, and Timers

  1. Arbotix, Arduino, and Timers

    So I recently got an Arbotix to replace my MiniRobocontroller as I was out of pins and needed the extra serial port. Now my code worked on the MiniRobocontroller. The Motors library was using Timer0, the Hservo library was using Timer1, an I had the following code using Timer2 to generate 1ms interrupts.

    Code:
     // First disable the timer overflow interrupt while we're configuring
      TIMSK2 &= ~(1<<TOIE2);  
      // Configure timer2 in normal mode (pure counting, no PWM etc.)
      TCCR2A &= ~((1<<WGM21) | (1<<WGM20));  
      TCCR2B &= ~(1<<WGM22);  
      // Select clock source: internal I/O clock
      ASSR &= ~(1<<AS2);  
      // Disable Compare Match A interrupt enable (only want overflow)
      TIMSK2 &= ~(1<<OCIE2A);  
      // Now configure the prescaler to CPU clock divided by 128
      TCCR2B |= (1<<CS22)  | (1<<CS20); // Set bits  
      TCCR2B &= ~(1<<CS21);             // Clear bit  
      /* We need to calculate a proper value to load the timer counter. 
       * The following loads the value 131 into the Timer 2 counter register 
       * The math behind this is: 
       * (CPU frequency) / (prescaler value) = 125000 Hz = 8us. 
       * (desired period) / 8us = 125. 
       * MAX(uint8) + 1 - 125 = 131; 
       */
      // Save value globally for later reload in ISR
      tcnt2 = 131;   
      // Finally load end enable the timer
      TCNT2 = tcnt2;  
      TIMSK2 |= (1<<TOIE2);
    and my ISR:

    Code:
    ISR(TIMER2_OVF_vect)
    {  
      // Reload the timer
      TCNT2 = tcnt2;  
      // increment the system_timer
      system_time = system_time++;
    }

    My code doesn't make use of arduino's mills(), micro(), or delay() functions, but am I correct in thinking that using all three timers would have broken these?

    So the Arbotix uses Timer2 for its motor driver library, which means I needed to switch my 1ms interrupt over to Timer0. I modified my code to look like this:

    Code:
     // First disable the timer overflow interrupt while we're configuring
      TIMSK0 &= ~(1<<TOIE0);  
      // Configure timer2 in normal mode (pure counting, no PWM etc.)
      TCCR0A &= ~((1<<WGM01) | (1<<WGM00));  
      TCCR0B &= ~(1<<WGM02);  
      // Select clock source: internal I/O clock
      ASSR &= ~(1<<AS2);  
      // Disable Compare Match A interrupt enable (only want overflow)
      TIMSK2 &= ~(1<<OCIE2A);  
      // Now configure the prescaler to CPU clock divided by 128
      TCCR0B |= (1<<CS22)  | (1<<CS20); // Set bits  
      TCCR0B &= ~(1<<CS21);             // Clear bit  
      /* We need to calculate a proper value to load the timer counter. 
       * The following loads the value 131 into the Timer 2 counter register 
       * The math behind this is: 
       * (CPU frequency) / (prescaler value) = 125000 Hz = 8us. 
       * (desired period) / 8us = 125. 
       * MAX(uint8) + 1 - 125 = 131; 
       */
      // Save value globally for later reload in ISR
      tcnt0 = 131;   
      // Finally load end enable the timer
      TCNT0 = tcnt0;  
      TIMSK0 |= (1<<TOIE0);
    With this ISR:

    Code:
    ISR(TIMER0_OVF_vect)
    {  
      // Reload the timer
      TCNT0 = tcnt0;  
      // increment the system_timer
      system_time = system_time++;
    }
    When I try to compile I get this error:

    core.a(wiring.c.o): In function `__vector_18':
    /Users/jeffreydamelio/Documents/Arduino/hardware/arbotix/cores/arbotix/wiring.c:45: multiple definition of `__vector_18'
    Sparky_1_0_arduino22.cpp.o:Sparky_1_0_arduino22.cp p:207: first defined here


    As near as I can tell, the file that modifies Millis(), micro(), etc. for use on the 644p is already trying to use this interrupt vector. Is this correct? What do I change to make this work? And thanks in advance to all the helpful people.

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    128

    Re: Arbotix, Arduino, and Timers

    Timer0 is used by Arduino to generate their system clock, so wiring.c includes a Timer0 overflow interrupt already. This is one of the reasons the ArbotiX switched to using Timer2 for motors, we can change the timer clock frequency to get higher-frequency PWM without screwing up the system clock.

    To make your code work, you'll either have to disable the Arduino system clock (besides breaking millis(), etc, not sure what implications this has), or do some sort of trickery with Timer2 to support both the motor PWM and your clock.

    Out of curiosity, why did you need your own system clock?

    -Fergs

  3. Re: Arbotix, Arduino, and Timers

    I just had systemtime in my ISR incrementing every 1ms for use in timing things in my various tasks, as I have multiple things going on that need to be timed but are really not at all picky about accuracy. I wasn't aware that Arduino already had something similar going on, and while I don't need their mills() etc. I don't really feel like risking messing up other things. Can I accomplish this same sort of timing using Arduino's system clock?

  4. Re: Arbotix, Arduino, and Timers

    Actually this is exactly what mills() is for isn't it... derp.

    I feel like there was some reason I didn't do this initially, but I don't remember it now. Oh well.

  5. Re: Arbotix, Arduino, and Timers

    Ok, heres another thing I can't find the answer for. The pinout on the Arbotix is confusing me. If for example I wanted to do an analog read on A7, analogRead(7); works, but I'm having trouble seeing the pattern. If all I give it is 7, how does it know I'm talking about the analog pin 7 and not the digital pin 7? What if I want to do a digitalRead on A7? None of the wiring diagrams seem to quite match what is actually working for me.

  6. #6
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    128

    Re: Arbotix, Arduino, and Timers

    Quote Originally Posted by draikani View Post
    Ok, heres another thing I can't find the answer for. The pinout on the Arbotix is confusing me. If for example I wanted to do an analog read on A7, analogRead(7); works, but I'm having trouble seeing the pattern. If all I give it is 7, how does it know I'm talking about the analog pin 7 and not the digital pin 7? What if I want to do a digitalRead on A7? None of the wiring diagrams seem to quite match what is actually working for me.
    The analogRead function only knows about analog pins, which are number 0-7.

    The trick to using digitalRead() is that DIGITAL = 31 - ANALOG for the analog pins, that is, analog 0 is digital 31. This is a left over annoyance from the Sanguino standard. Arduino recently introduced the notion of using "digitalRead(A7)" where A7 would be defined to be the correct digital pin, however, this is not yet in a release of ArbotiX (it is available in trunk of SVN, and will be available in our next release).

    -Fergs

  7. Re: Arbotix, Arduino, and Timers

    Thanks for the quick replies Fergs, really makes the Arbotix a pleasure to use. So one more question, what do I need to do to use the second serial port as a regular serial port? I'm trying to use it with spark fun's serial lcd backpack. I tried Serial1.begin(9600); and got:

    Sparky_1_0_arduino22:759: error: 'Serial1' was not declared in this scope

    This is because the Arbotix sets it aside for Bioloid things right?
    Last edited by draikani; 04-07-2012 at 08:49 PM.

  8. Re: Arbotix, Arduino, and Timers

    Ok so I modified the hardwareserial.h and hardwareserial.cpp files by uncommenting the lines related to Serial1, and adding a line defining rx_buffer1. Now it sort of works, but it's being very finicky. I have to power up the Arbotix with the FTDI chip disconnected, then plug it in, then reset the arbotix. Even if I don't intend to use the FTDI chip I still have to power on and then reset. Am I at least on the right track here?
    Last edited by draikani; 04-07-2012 at 08:51 PM.

  9. Re: Arbotix, Arduino, and Timers

    oops double

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Arduino- xbee -xbee-arduino - stepper motors
    By Icemonkey in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 06-04-2012, 12:35 PM
  2. Question(s) ArbotiX and Arduino ADK compatibility
    By phantomDroidX in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 01-18-2012, 05:39 PM
  3. Question(s) arbotix and arduino pro
    By Bunkerman in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 05-01-2011, 10:56 PM
  4. SOLVED: Arbotix + Arduino IDE + Ubuntu + Invalid Device Sig
    By cdraptor in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 01-22-2011, 06:34 PM
  5. PVision library for Arduino (Pixart/Wiimote to Arduino)
    By shobley in forum Robot Computers
    Replies: 1
    Last Post: 03-01-2009, 05:07 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •