Page 1 of 2 12 LastLast
Results 1 to 10 of 16

Thread: 2012 MWScore FSR Target Panel Build Tutorial & Info

  1. #1
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    2012 MWScore FSR Target Panel Build Tutorial & Info

    Going to break this into two main sections: Full sized and Half Size FSR Target Panels. I recommend reading all of this first (both sections) before attempting anything.

    Please refer to Section VII of the Ruleset thread for mounting guidelines. Make sure you route your target panel cables away from sources of EMF (gun motors are a notorious culprit). Also, having your target panels mounted too closely to your guns can cause problem. Make sure you test firing and running around with your scoring system mounted to make sure you won't have problems at the competition.

    Ensure all cables and target panels are securely fastened, target panels falling off will count as 1 point of damage. If a cable falls out you'll start taking damage very quickly due to it being an open collector. I recommend using a heavy duty velcro or even 3M Dual Lock/Radio Shack Super Lock velcro (be careful when using this stuff if you need to remove a target panel, it has a LOT of grip).

    Full Size FSR Target Panels

    1) Here are the parts for a Full Size Panel. Learn them, love them. The black ABS is your back plate, the clear lexan is the front plate that protects the FSRs. FSRs go in between the black ABS and clear lexan plates. The PCB attachs to the back plate. But don't start building yet! Let's go over everything step by step.
    Click image for larger version. 

Name:	Img3769.jpg 
Views:	622 
Size:	41.4 KB 
ID:	3900

    2) Prepare the lexan plates by peeling off the plastic protective film. Set these lexans plates aside for later.
    Click image for larger version. 

Name:	Img3772.jpg 
Views:	542 
Size:	39.7 KB 
ID:	3901

    3) If you have back plates that have a textured side, the FSRs are mounted on the smooth side.
    Click image for larger version. 

Name:	Img3776.jpg 
Views:	552 
Size:	35.1 KB 
ID:	3902

    4) First we need to mount the FSRs to the black ABS back plates. Peel them ONE AT A TIME.
    Click image for larger version. 

Name:	Img3782.jpg 
Views:	535 
Size:	31.6 KB 
ID:	3908

    5) Very carefully align the first FSR. Use the edges of the back plate to line it up correctly. Please be very careful during this, you do not want to misalign the FSRs and have them hanging off the edge/too far in from the edge. Once you stick these on, they do NOT come off, so you only have one shot.
    Click image for larger version. 

Name:	Img3777.jpg 
Views:	531 
Size:	45.9 KB 
ID:	3903

    6) Your first FSR should look like this.
    Click image for larger version. 

Name:	Img3778.jpg 
Views:	552 
Size:	31.0 KB 
ID:	3904

    7) Peel & prepare the second FSR. Align this with the top edge (in this pic) of the back plate, and the center axis right up against the edge of the first (already mounted) FSR.
    Click image for larger version. 

Name:	Img3779.jpg 
Views:	511 
Size:	49.0 KB 
ID:	3905Click image for larger version. 

Name:	Img3780.jpg 
Views:	545 
Size:	44.5 KB 
ID:	3906

    8) It should look like this if done correctly. If it doesn't look like this, cry. You've disappointed your ancestors.
    Click image for larger version. 

Name:	Img3781.jpg 
Views:	559 
Size:	34.0 KB 
ID:	3907

    9) Carefully align the 3rd FSR. Again, make sure its snug up against the adjacent FSR, and the bottom (in this pic) edge of the back plate.
    Click image for larger version. 

Name:	Img3783.jpg 
Views:	530 
Size:	56.8 KB 
ID:	3909Click image for larger version. 

Name:	Img3784.jpg 
Views:	537 
Size:	43.3 KB 
ID:	3910

    10) Carefully align the 4th FSR. Make sure its snug up against the adjacent FSRs.
    Click image for larger version. 

Name:	Img3785.jpg 
Views:	489 
Size:	57.7 KB 
ID:	3911Click image for larger version. 

Name:	Img3786.jpg 
Views:	503 
Size:	40.3 KB 
ID:	3912

    11) These be the parts for your FSR PCB. Word.
    Click image for larger version. 

Name:	Img3789.jpg 
Views:	578 
Size:	30.2 KB 
ID:	3913

    12) Install your components as shown. Note, resistors may be tan or blue, 4.7k-5.1k resistance. Solder the components.
    Click image for larger version. 

Name:	Img3793.jpg 
Views:	541 
Size:	47.5 KB 
ID:	3914Click image for larger version. 

Name:	Img3791.jpg 
Views:	557 
Size:	45.5 KB 
ID:	3915

    13) Apply double sided sticky tape (not included, you cheap bastards). Make sure you use some high-strength stuff. DO NOT ATTACH THE PCB YET.
    Click image for larger version. 

Name:	Img3794.jpg 
Views:	522 
Size:	41.9 KB 
ID:	3916

    14) Without actually attaching the PCB, carefully insert all 4 FSR leads into the PCB as shown. Take your time with this, and be gentle.
    Click image for larger version. 

Name:	Img3797.jpg 
Views:	609 
Size:	71.9 KB 
ID:	3917

    15) Again, before attaching the PCB to the back plate, carefully solder the FSR leads to the PCB. Use low temperatures (375F) and do not hold the iron on any connection for more than 3 seconds. You will melt the FSR connections if you get too heavy handed.
    Click image for larger version. 

Name:	Img3799.jpg 
Views:	525 
Size:	58.1 KB 
ID:	3918

    16) Very carefully bend the connections flat. CAREFUL. Be a gentle lover.
    Click image for larger version. 

Name:	Img3800.jpg 
Views:	540 
Size:	47.1 KB 
ID:	3919

    17) Attach the PCB to the back plate with steady applied pressure.
    Click image for larger version. 

Name:	Img3801.jpg 
Views:	526 
Size:	80.0 KB 
ID:	3920


    18) Voila!
    Click image for larger version. 

Name:	Img3802.jpg 
Views:	530 
Size:	65.2 KB 
ID:	3921

    19) Line up the lexan plate.
    Click image for larger version. 

Name:	Img3803.jpg 
Views:	543 
Size:	54.6 KB 
ID:	3922

    20) Use tape (electrical is what I use) of your choice to attach the lexan plate, along the edge and around to the back plate.
    Click image for larger version. 

Name:	Img3804.jpg 
Views:	529 
Size:	91.2 KB 
ID:	3923Click image for larger version. 

Name:	Img3806.jpg 
Views:	539 
Size:	86.8 KB 
ID:	3924

    21) Attach velcro to the PCB in preparation for mounting.
    Click image for larger version. 

Name:	Img3807.jpg 
Views:	537 
Size:	63.0 KB 
ID:	3925Click image for larger version. 

Name:	Img3808.jpg 
Views:	533 
Size:	68.7 KB 
ID:	3926

    22) Look! Cable! Ready! I highly recommend putting a dab of glue on header/cable connection here to make sure it doesn't wiggle loose. You can remove the buckle from the cable if you like. The side that plugs into the transponder needs to be unbuckled.

    Please note S, V, G.
    S = Yellow/White, V = Red, G = Black.
    Click image for larger version. 

Name:	Img3829.jpg 
Views:	576 
Size:	55.3 KB 
ID:	3944

    Half Size (Split-Option) FSR Target Panels

    NOTE: These instructions are for Half-Size FSR Target Panels that are used for the 'split option'. This method utilizes a single PCB that is split in two, and a tether between the two half-size panels, which are then connected to the MWScore Transponder using a single cable.

    If you have questions, ask. Again, read everything before proceeding, if you're building a biped make sure you understand the difference.

    1) Here are the parts for a Half Size Panel. Learn them, love them. The black ABS is your back plate, the clear lexan is the front plate that protects the FSRs. FSRs go in between the black ABS and clear lexan plates. The PCB attachs to the back plate. But don't start building yet! Let's go over everything step by step.
    Click image for larger version. 

Name:	Img3813.jpg 
Views:	537 
Size:	47.7 KB 
ID:	3929

    2) Use a ruler to score the PCB, several times. You don't need to press hard, just apply firm pressure and score it 5-6 times. You should be able to line it up to the edge of a table and snap it with your hands. I recommend sanding the scored edge so it doesn't get fiberglass fibers everywhere.
    Click image for larger version. 

Name:	Img3810.jpg 
Views:	528 
Size:	54.8 KB 
ID:	3927Click image for larger version. 

Name:	Img3811.jpg 
Views:	525 
Size:	23.5 KB 
ID:	3928

    2) Prepare the lexan plates by peeling off the plastic protective film. Set these lexans plates aside for later.
    Click image for larger version. 

Name:	Img3814.jpg 
Views:	494 
Size:	41.8 KB 
ID:	3930

    3) If you have back plates that have a textured side, the FSRs are mounted on the smooth side.
    Click image for larger version. 

Name:	Img3816.jpg 
Views:	499 
Size:	28.8 KB 
ID:	3931

    4) First we need to mount the FSRs to the black ABS back plates. Peel them ONE AT A TIME.
    Click image for larger version. 

Name:	Img3782.jpg 
Views:	535 
Size:	31.6 KB 
ID:	3908

    5) Very carefully align the first FSR. Use the edges of the back plate to line it up correctly. Please be very careful during this, you do not want to misalign the FSRs and have them hanging off the edge/too far in from the edge. Once you stick these on, they do NOT come off, so you only have one shot.
    Click image for larger version. 

Name:	Img3817.jpg 
Views:	515 
Size:	37.8 KB 
ID:	3932

    6) Align and mount the 2nd FSR.
    Click image for larger version. 

Name:	Img3818.jpg 
Views:	520 
Size:	40.6 KB 
ID:	3933Click image for larger version. 

Name:	Img3823.jpg 
Views:	533 
Size:	45.7 KB 
ID:	3938Click image for larger version. 

Name:	Img3824.jpg 
Views:	521 
Size:	34.5 KB 
ID:	3939

    7) Place the components as follows.
    Click image for larger version. 

Name:	Img3819.jpg 
Views:	535 
Size:	24.7 KB 
ID:	3934

    8) Solder them.
    Click image for larger version. 

Name:	Img3820.jpg 
Views:	518 
Size:	23.2 KB 
ID:	3935Click image for larger version. 

Name:	Img3821.jpg 
Views:	513 
Size:	22.0 KB 
ID:	3936

    9) Apply double sided sticky tape (not included, you cheap bastards). Make sure you use some high-strength stuff. DO NOT ATTACH THE PCB YET.
    Click image for larger version. 

Name:	Img3822.jpg 
Views:	534 
Size:	36.2 KB 
ID:	3937

    10) Without actually attaching the PCB, carefully insert 2 FSR leads into the PCB as shown. Take your time with this, and be gentle. Repeat for the other side.
    Click image for larger version. 

Name:	Img3823.jpg 
Views:	533 
Size:	45.7 KB 
ID:	3938Click image for larger version. 

Name:	Img3825.jpg 
Views:	534 
Size:	56.3 KB 
ID:	3940

    11) Again, before attaching the PCB to the back plate, carefully solder the FSR leads to the PCB. Use low temperatures (375F) and do not hold the iron on any connection for more than 3 seconds. You will melt the FSR connections if you get too heavy handed.
    Click image for larger version. 

Name:	Img3826.jpg 
Views:	537 
Size:	55.8 KB 
ID:	3941

    12) Very carefully bend the connections flat. CAREFUL. Be a gentle lover.
    Click image for larger version. 

Name:	Img3827.jpg 
Views:	528 
Size:	48.1 KB 
ID:	3942

    13) Attach the PCB to the back plate with steady applied pressure.
    Click image for larger version. 

Name:	Img3828.jpg 
Views:	524 
Size:	41.1 KB 
ID:	3943

    14) Attach the lexan plate to the front using the same taping method described in the last section.
    Click image for larger version. 

Name:	Img3833.jpg 
Views:	530 
Size:	25.1 KB 
ID:	3948

    15) Velcro, do it.
    Click image for larger version. 

Name:	Img3830.jpg 
Views:	543 
Size:	54.0 KB 
ID:	3945

    16) This is how the cabling works for the split-option Half-Size FSR Target Panel set. You can shorten the tether cable between the two panels as much as you need. I highly recommend putting a dab of glue on header/cable connection here to make sure it doesn't wiggle loose. You can remove the buckle from the cable if you like. The side that plugs into the transponder needs to be unbuckled.

    Please note S, V, G.
    S = Yellow/White, V = Red, G = Black.
    Click image for larger version. 

Name:	Img3831.jpg 
Views:	546 
Size:	48.5 KB 
ID:	3946


    MWScore Transponder Pinout

    Click image for larger version. 

Name:	Img3836.jpg 
Views:	719 
Size:	60.5 KB 
ID:	3951

    We do not recommend powering these directly from an 11.1v (12.6v max) 3S Lipo. They can be powered directly off of a 5v pin from the arbotix without issue however.

    Please note: If you ordered Xbees you will need to program them appropriately. Each one of you has a unique ID # (it's written on your MWScore transponder), this is important when setting up your Xbees.

    Xbee info:

    ATBD = 5 (38400bps)
    ATID = 6200
    MY = 6200 + TRANSPONDER_ID_NUMBER (written on the bottom of each transponder)
    DL = 6201
    CH = c

    If you don't have a method of programming your Xbees, bring them to Robogames and we'll get you programmed before your qualification round. Make sure to get this done early, it's your responsibility.

    Wiring examples:
    Click image for larger version. 

Name:	Img3834.jpg 
Views:	589 
Size:	49.6 KB 
ID:	3949Click image for larger version. 

Name:	Img3835.jpg 
Views:	620 
Size:	63.7 KB 
ID:	3950
    Last edited by DresnerRobotics; 03-12-2013 at 04:33 PM.

  2. #2
    Join Date
    Sep 2008
    Location
    Toronto, Ontario
    Posts
    171
    Images
    43
    Rep Power
    41

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    I played with reading the hit information from my Arbotix over the weekend and here's the gist of the code to do it.

    Code:
    void setup( )
    {
      Serial.begin( 38400 );    
      pinMode( 0, OUTPUT );
      delay( 250 );
    
    
      pinMode( A1, INPUT );
      delay( 250 );
    }
    
    
    void loop()
    {
      unsigned long duration;
    
    
      duration = pulseIn( A1, LOW, 300000 );
      if( duration > 0 ) {
        if( duration < 50000 ) {
          Serial.println( "Hit panel 1" );
        } else if( duration < 100000 ) {
          Serial.println( "Hit panel 2" );
        } else if( duration < 150000 ) {
          Serial.println( "Hit panel 3" );
        } else if( duration < 200000 ) {
          Serial.println( "Hit panel 4" );
        }
      }
    }
    Cheers!


  3. #3
    Join Date
    May 2010
    Location
    Princeton University
    Posts
    354
    Rep Power
    38

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    Thanks for posting that. Saves me a bit of time figuring it out myself... if I manage to get things running smoothly enough to add things like that.

  4. #4
    Join Date
    May 2010
    Location
    Princeton University
    Posts
    354
    Rep Power
    38

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    I already posted this in the ordering thread. Sorry to repost, but not having an answer to this is really holding up my work.

    I've given up on my current set of target panels. After tweaking them continually to make them mount better, they are looking pretty shabby. I plan to switch to placing my pcbs remotely and using female header fsrs. However, my pcbs and panels are not in great shape. They are usable with some maintenance, but replacement would be a much better option. Any way I could get 4 panels and 4 pcbs? If not, I can easily make my own circuits to replace the pcbs and make my own panels. Would that be legal? Just checking. Thanks.

  5. #5
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    Quote Originally Posted by byi View Post
    I already posted this in the ordering thread. Sorry to repost, but not having an answer to this is really holding up my work.

    I've given up on my current set of target panels. After tweaking them continually to make them mount better, they are looking pretty shabby. I plan to switch to placing my pcbs remotely and using female header fsrs. However, my pcbs and panels are not in great shape. They are usable with some maintenance, but replacement would be a much better option. Any way I could get 4 panels and 4 pcbs? If not, I can easily make my own circuits to replace the pcbs and make my own panels. Would that be legal? Just checking. Thanks.
    You must build these exactly as specified. I can't have people with variations on the scoring system, it all has to be exactly as specified.

    The reason I've strayed away from female FSRs is because I don't want the chance of the individual FSRs coming apart. I don't want to trust people gluing them either.

    I can most certainly send you PCBs and panels. What version did you have? In the future, feel free to email me with requests like this (I don't recall receiving an email from you). I've been very busy lately and thus haven't been on the phone much.

    FSR panels are intended to be a consumable. I really only expect 2 years of use out of them. With that said, the newer versions are much more robust as they have the FSR ribbons protected now.

  6. #6
    Join Date
    May 2010
    Location
    Princeton University
    Posts
    354
    Rep Power
    38

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    I got mine shortly before robogames 2011, so I think they are the newer ones. I'll email you immediately. Thanks for the help.

  7. #7
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    43

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    My panels from last year were showing a bit of damage, but still worked. Decided to make them a bit more resistant to having the cables crushed, and used a chopped up pen barrel and hot glue to provide protection to the FSRs' ribbon wires.
    Click image for larger version. 

Name:	mwscorepaneltip.jpg 
Views:	1206 
Size:	66.5 KB 
ID:	4574

  8. #8

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    1) so in the instructions - should that be (375C) not 375F for soldering?

    2) Also just an update on the transponder? - the directions on this forum mention 5v not 11.1, however on the transponder store page it says
    7-24v voltage input which is what I remembered from 2012.

  9. #9

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    Actually, a typical melting temperature for Tin/Lead solder is 370 Farenheit, so I believe the suggestion is to go as low as you can while still getting melt.

  10. #10

    Re: 2012 MWScore FSR Target Panel Build Tutorial & Info

    Well, I started at 375F and could not getting anything to melt with my thinnest solder until around 600F. It did not seem to melt the wires or anything but I did not let it linger long.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Arduino Robot Tutorial/ROS
    By Atom in forum ROS - Robot Operating System
    Replies: 3
    Last Post: 07-11-2011, 04:16 AM
  2. Mini RoboController /Target Panel Setup
    By elaughlin in forum Mech Warfare
    Replies: 10
    Last Post: 12-12-2010, 10:30 PM
  3. Control Panel for PC / Xbee
    By Robot Dude in forum Mech Warfare
    Replies: 11
    Last Post: 09-28-2009, 07:50 PM
  4. BB sensor tutorial
    By ScuD in forum Off Topic
    Replies: 3
    Last Post: 01-26-2009, 03:44 PM
  5. HA tutorial???
    By Vaughn in forum Software and Programming
    Replies: 5
    Last Post: 11-07-2007, 02:09 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •