Results 1 to 4 of 4

Thread: NUKE and Test Drive

  1. NUKE and Test Drive

    When using the NUKE test drive button, moving the sliders moves my robots servos to fixed positions and then stops. However, from the NUKE introduction video (seen here around 7:00 - http://www.youtube.com/watch?v=biA7AhWRvpU), it looks like it is supposed to give continuous motion. Is there something I'm missing, or doing wrong?

    Also, I noticed that two of the robots legs seem to work fine, but the other two don't work as expected. I looked into nuke.cpp, and found this:

    int mins[] = {286, 518, 234, 289, 209, 254, 274, 0, 160, 301, 210, 132};
    int maxs[] = {701, 589, 794, 732, 815, 805, 739, 512, 759, 709, 816, 750};

    I'm assuming that these are in servo id order (1-12). This would explain why two of the legs (servos 1,2,3 and 7,8,9) are not working correctly: they either have very limited ranges (518-589 for servo 2), or abnormal ranges (0-512 for servo 8, compared to the others which have 210-816). When configuring the extremes I took extra cafe to make sure that the the legs all had roughly the same exteremes, so why would some of the them have completely different values?

    Thanks in advance for the help.

  2. #2
    Join Date
    Sep 2010
    Posts
    183
    Images
    16
    Rep Power
    33

    Re: NUKE and Test Drive

    You are correct in assuming those are the limits for servo 1-12 in order.

    You may have messed up on one of the servo's when doing pypose, i had to do it several times the first time i went through it to get everything correct. You could manually edit the servo's to have similar values to the other legs that are in the same configuration. On my quad i manually edited these values after the fact, but be careful since you could run your servo's into another part of the robot and damage them.

  3. Re: NUKE and Test Drive

    Thanks for the help. Part of the problem was that two of the attachments for our motors were added at 90 degree angles from what "neutral" was.

    However, I have found that on startup, when the robot tries to "stand", the legs move far outside the min and max values (legs will touch, even though I calibrated to make sure it couldn't happen). Is the standing postion the same as neutral, or is it something else? If its something else, is there a way to configure it? Thanks.

  4. #4
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    121

    Re: NUKE and Test Drive

    Quote Originally Posted by meakero View Post
    Thanks for the help. Part of the problem was that two of the attachments for our motors were added at 90 degree angles from what "neutral" was.

    However, I have found that on startup, when the robot tries to "stand", the legs move far outside the min and max values (legs will touch, even though I calibrated to make sure it couldn't happen). Is the standing postion the same as neutral, or is it something else? If its something else, is there a way to configure it? Thanks.
    There are dozens of ways the configuration could be wrong -- the fastest way to get to the bottom of this is to post your .ppr file and a picture of your robot in the neutral pose.

    -Fergs

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Anyone using omnidirectional drive?
    By Pi Robot in forum Rovers
    Replies: 56
    Last Post: 05-18-2012, 02:08 PM
  2. PhantomX Hexapod with Nuke - Question on how I am using it
    By cdraptor in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 04-11-2012, 04:01 AM
  3. Announcing NUKE
    By lnxfergy in forum Software and Programming
    Replies: 20
    Last Post: 06-15-2010, 12:08 PM
  4. Drive Control
    By Remus in forum Rovers
    Replies: 3
    Last Post: 11-16-2008, 01:31 PM
  5. FREE Robot Test Drive
    By RobotServicesGroup in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 11-14-2008, 07:53 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •