Thanks Zenta,
I am merging now... I totally understand... Not sure yet about the changes for Tibia Min/Max if this is safe for default ones as well, will probably simply create a:
#define OPTION_UPSIDE_DOWN
when define:
and depending on if it is defined will set some variables differently...
versusCode:#define cRRTibiaMin1 -1500 #define cRRTibiaMax1 1500
KurtCode:#define cXXTibiaMin1 -700 #define cXXTibiaMax1 900



Reply With Quote


showing the robot taking a couple of steps and then I grab the robot and start to turn it over and the legs all move to the other side and then I put it down and have it walk again...


Bookmarks