Trossen Desktop RoboTurret Top Banner
+ Reply to Thread
Results 1 to 2 of 2

Thread: How to decide run current and hold current in stepper motor

  1. How to decide run current and hold current in stepper motor

    I am programming a motor controller where I have to specify the run current (coil peak current) and hold current (coil hold current) of the motors. The motor I used is a bipolar stepper motor, with a whopping 1.86Kg/cm of stall torque at 1.5Amp current (0.75A per winding) at 1.8 degree stepping angle.However, the table in the specification makes me confused: It lists a different current for a different torque.Here is a link to that motor controller http://www.nex-robotics.com/products...per-motor.html.How could I determine run current and hold current from this specification?
    Last edited by KevinQ; 05-01-2012 at 03:29 PM.

  2. #2

    Re: How to decide run current and hold current in stepper motor

    That table says something like:

    "If you want this torque, then you need to supply at least this many volts, and that means the motor will draw this many amps."

    So, it's up to you. Do you want to run the motor full throttle? Then provide at least 6V, and limit amps to 1.5. (This divides out with PWM, too, so 6V, 3A, at 50 % duty cycle may give similar results.)
    Generally, for a driver, though, you want to provide a lot more voltage, and instead limit current, using a chopping driver. And, reading that data sheet, any "max current" setting of 1.5A or lower, per winding, should be safe. Higher would probably be possible, but wouldn't be recommended for any long durations or high duty cycles.

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. current limit
    By gradstudent21 in forum I/O Boards and Controllers
    Replies: 0
    Last Post: 11-22-2011, 10:19 AM
  2. Question(s) How do I cause a dc motor to hold itself at its current position?
    By Rick in forum Robotics General Discussion
    Replies: 26
    Last Post: 04-11-2009, 12:35 PM
  3. High Current Motor Controller
    By Sienna in forum I/O Boards and Controllers
    Replies: 1
    Last Post: 11-10-2008, 10:59 AM
  4. Question(s) Undervolting motors and current-draw?
    By Adrenalynn in forum Robotics General Discussion
    Replies: 23
    Last Post: 05-08-2008, 11:01 AM
  5. Does this stepper motor need a driver?
    By Adman in forum I/O Boards and Controllers
    Replies: 4
    Last Post: 03-20-2008, 10:26 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts