Trossen Hexapod  Top Banner
+ Reply to Thread
Page 2 of 2 FirstFirst 12
Results 11 to 16 of 16

Thread: PDF is unreadable - Robot Controller Joystick - Medium -3D

  1. #11
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    829
    Images
    20
    Rep Power
    38

    Re: PDF is unreadable - Robot Controller Joystick - Medium -3D

    Quote Originally Posted by tician View Post
    maybe "97.1" for the total height
    gah, over estimated by 3 mm.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"

  2. Re: PDF is unreadable - Robot Controller Joystick - Medium -3D

    Ahhhh, beautiful pixels! So relaxing!

    Thanks so much!

    Quote Originally Posted by Tyberius View Post
    Working on getting this fixed ASAP. I'll let you know. Thanks for pointing it out, something got messed up when we generated the PDF and it wasn't apparent without zooming in.

    Also, blame Kyle.

    Edit: FIXED

  3. Re: PDF is unreadable - Robot Controller Joystick - Medium -3D

    Any measures on the bezel mount? Looks like 32.5x32.5mm


    Quote Originally Posted by coreyfro View Post
    Ahhhh, beautiful pixels! So relaxing!

    Thanks so much!

  4. Re: PDF is unreadable - Robot Controller Joystick - Medium -3D

    Hey, does any one know how to remove the knob for mounting this joy stick? Is there a set screw somewhere? Is the rubber grip removable? Is there some tricky way to get in through the base?

    The bellows are really nice, but they make it tough to mount without pulling the knob off...

  5. #15
    Join Date
    Dec 2007
    Location
    Trossen Robotics
    Posts
    3,036
    Images
    933
    Rep Power
    103

    Re: PDF is unreadable - Robot Controller Joystick - Medium -3D

    Quote Originally Posted by machineherder View Post
    Hey, does any one know how to remove the knob for mounting this joy stick? Is there a set screw somewhere? Is the rubber grip removable? Is there some tricky way to get in through the base?

    The bellows are really nice, but they make it tough to mount without pulling the knob off...
    The main hole for mounting these should be approximately the diameter of the gimbal, which is slightly larger than the knob (of the 3 axis one). You shouldn't need to remove the knob to mount these at all if you're making your holes the correct size (I've mounted both types in a custom controller, used a 38mm hole).
    Andrew Alter
    Trossen Robotics
    R&D Lead
    Join the Robotic Combat Revolution @ Mech Warfare!

  6. Re: PDF is unreadable - Robot Controller Joystick - Medium -3D

    I realized my mistake. I didn't realize that the ring was removable.

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. Robot Controller, Relays, Speed Controllers
    By Parts in forum Garage Sale
    Replies: 4
    Last Post: 03-17-2012, 01:50 PM
  2. Project Robot Controller
    By Quantum in forum Project Showcase
    Replies: 20
    Last Post: 02-23-2012, 08:15 PM
  3. Handheld Robot Controller
    By jdolecki in forum Robotics General Discussion
    Replies: 1
    Last Post: 10-25-2010, 07:43 PM
  4. Question(s) PDA Controller robot design questions
    By xntx in forum I/O Boards and Controllers
    Replies: 4
    Last Post: 05-05-2010, 03:05 PM
  5. Project Custom joystick to control robot arm
    By HakBot in forum Project Showcase
    Replies: 22
    Last Post: 08-22-2008, 10:44 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts