Trossen Force Sensor  Top Banner
+ Reply to Thread
Results 1 to 6 of 6

Thread: where in the Arbotix AVR code is it talking to the XBEE serial port?

  1. #1

    where in the Arbotix AVR code is it talking to the XBEE serial port?

    Ok, I'm making slow progress on my bluetoothed android phone to bluetooth bee'd arbotix board.
    Almost got the android app to pair to another and sending back and forth some text.
    Then I try android=>bluetooth bee=>arbotix.


    I went browsing through arbotix-0014.zip and couldn't find WHERE in the heck it's talking to the
    X BEE's serial port.
    Can somebody point that out to me, please? Like a .c filename and path within that arbotix-0014 dir?

    From what I'm gathering, ya have one little arduino app on the AVR and it doesn't change much if at all.
    It's loading servo specs=>flash=>XBEE serial port=>other PC connected XBEE=>pythonSerial_WhateverYaCallIt=>python GUI, right?

    I see where it's doing the AX12 serial bus. But not where it's messing with the XBEE one??

    thanks for any pointers,

    ...Steve

  2. #2
    Join Date
    Dec 2007
    Location
    Trossen Robotics
    Posts
    3,019
    Images
    910
    Rep Power
    103

    Re: where in the Arbotix AVR code is it talking to the XBEE serial port?

    Check the Commander library. It's inside the Robocontroller library (which I believe is going to be merged with the Arbotix library soon).
    Andrew Alter
    Trossen Robotics
    R&D Lead
    Join the Robotic Combat Revolution @ Mech Warfare!

  3. Re: where in the Arbotix AVR code is it talking to the XBEE serial port?

    An XBEE is just a serial device -- it's the default Serial on the arbotix. If you're using the PyPose sketch as a reference, it makes calls directly to Serial.read/write() in the sketch. If you're using a NUKE-exported sketch, it uses the Commander library (part of http://code.google.com/p/robocontroller/).

    -Fergs

  4. Trossen Arduino Thread Banner
  5. #4

    Re: where in the Arbotix AVR code is it talking to the XBEE serial port?

    Ok, I got that Commander thingy.
    But =it= seems to use some HardwareSerial.h and probably some other .cpp files...

    Where do I come across THOSE babies?

    So where's the top level of all this arduino arbotix stuff?
    I found this arbotix/core/arbotix/main.cpp
    But how do I know what all tentacles are included in this thing?

    Thanks for your help tho - i REALLY appreciate it.
    I think a droided arbotix would be PRETTY dang cool...

  6. #5

    Re: where in the Arbotix AVR code is it talking to the XBEE serial port?

    ohhhhhhhh k. Those little .pde files are actually c++.
    I blew em all away lookin only for cpp

    This dang arduino business will probably drive me insane.
    Seems like in order to make cpp easier, they've made cpp harder (well, messier at least)

    Ok, I'm good - thanks mucho.

  7. #6
    Join Date
    Dec 2007
    Location
    Trossen Robotics
    Posts
    3,019
    Images
    910
    Rep Power
    103

    Re: where in the Arbotix AVR code is it talking to the XBEE serial port?

    Basically a lot of the integrated functions of the arduino IDE draw upon core 'arduino library' dependencies. Easier on the front end, but messier on the back end when you go digging through code.
    Andrew Alter
    Trossen Robotics
    R&D Lead
    Join the Robotic Combat Revolution @ Mech Warfare!

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. Question(s) Using a WRT54GL router with serial port
    By Sundsted in forum Software and Programming
    Replies: 0
    Last Post: 07-07-2010, 12:53 PM
  2. Serial Port in VBScript
    By Judge in forum Software and Programming
    Replies: 11
    Last Post: 01-04-2010, 08:12 AM
  3. Question(s) Cannot figure out how to write to the serial port in C++
    By Superlaxstar112 in forum Software and Programming
    Replies: 4
    Last Post: 07-23-2008, 05:02 PM
  4. For Sale Xbee Wireless Serial Setup
    By jbod in forum Robotics General Discussion
    Replies: 0
    Last Post: 04-15-2008, 06:35 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts