Results 1 to 7 of 7

Thread: Custom Aluminium 4DOF Hexapod For Sale

  1. Custom Aluminium 4DOF Hexapod For Sale

    Hi, I'm thinking of selling one of my custom built hexapods, however, if it doesn't sell I will strip it down and sell off the servos .. read on for more details.


    Picture of the Hexapod Next to a 300mm Ruler.



    This is the largest RC servo hexapod I have built so far, and had a 4 DOF leg design, with all the leg and body parts designed by myself using T6 grade aluminium and cut on my CNC router. The upper and lower body plates are 4mm thick, the leg plates are 2mm thick. The hexapod uses 24 dynamixel servos arranged in the following manner:


    Coxa: RX-10
    Femur: RX-28
    Tibia: RX-10
    Metatarsus: RX-10











    Each of the legs is cabled back to a central power and signal distribution PCB. The hexapod was built towards the end of 2009, and was used as a test platform for my 4-DOF algorithms and to test some foot sensors I was working on. All electronics for the hexapod have been removed. The hexapod worked fairly well, however, although the dynamixel servos have plenty of torque, I found their resolution of 1024 steps to be somewhat limiting for my tests, and after about 5 to 8 hours of use over several months the hexapod has been collecting dust. All servos are in good working order.





    The Foot design consists of a 8mm ball and custom machined delrin socket foot attached to a dynamixel bracket. The foot has an adhesive foam pad on the bottom.





    I thought I would see if anyone is interested in the platform before I break it down and sell the servos individually, as it seems a shame to waste all this engineering! Maybe you know a university or research institute that might be interested Feel free to pass on these details.





    If your interested in purchasing the hex, PM me with a sensible offer, bare in mind that the servos alone would cost in excess of £2500 GBP

  2. #2

    Re: Custom Aluminium 4DOF Hexapod For Sale

    I can't afford to buy your pod, even though it looks nice :-)

    A question, though: Do the springs really help? It seems like the load on the hip joints would be going the same way as the springs, so when "resting" with the body off the ground, wouldn't the springs actually work in the same direction as gravity?

  3. #3
    Join Date
    Jun 2011
    Location
    USA
    Posts
    533
    Images
    107
    Rep Power
    39

    Re: Custom Aluminium 4DOF Hexapod For Sale

    Just wanted to say... nice job on the construction and pretty pictures Thanks for sharing.

  4. Re: Custom Aluminium 4DOF Hexapod For Sale

    Quote Originally Posted by jwatte View Post
    I can't afford to buy your pod, even though it looks nice :-)

    A question, though: Do the springs really help? It seems like the load on the hip joints would be going the same way as the springs, so when "resting" with the body off the ground, wouldn't the springs actually work in the same direction as gravity?
    The springs do nothing while the hexapod is powered up, they were added just to stop the legs from collapsing as fast when picking the hexapod up when the servos are powered off. Although to be honest they didn't help that much.

  5. #5
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    138

    Re: Custom Aluminium 4DOF Hexapod For Sale

    Curious- do you have any video of this guy walking? Love the design!

  6. #6
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    77

    Re: Custom Aluminium 4DOF Hexapod For Sale

    Hi Matt,

    Its been awhile since I saw a render of your hex in 2009. Great to see some real pics of it! Looks great, very interesting foot design. You've not considered just selling the servos and replace them with the MX series?
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  7. Re: Custom Aluminium 4DOF Hexapod For Sale

    Quote Originally Posted by Tyberius View Post
    Curious- do you have any video of this guy walking? Love the design!
    Unfortunately not! I spent a substantial amount of time tweaking the code for this guy, but never bothered filming it! I'm now using a simulator instead which is easier to deal with, but not as nice to look at

    Its been awhile since I saw a render of your hex in 2009. Great to see some real pics of it! Looks great, very interesting foot design. You've not considered just selling the servos and replace them with the MX series?
    I could, but as mentioned above I now use a simulator. The MX series do look very good, although I'm not entirely convinced 12bit resolution is enough for good PID control. Have you tried them?

    The servos I have built myself for various animatronics jobs have at least 15bit feedback, as you tend to loose a bit or two with noise, and to get a decent velocity signal from them you need higher resolutions, unless you have a velocity encoder on the back of the motor

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. for sale pheonix hexapod
    By christinag in forum Garage Sale
    Replies: 3
    Last Post: 04-05-2012, 11:25 PM
  2. Contest Entry AluHex: 4DOF Hexapod on a Budget
    By r691175002 in forum Project Showcase
    Replies: 36
    Last Post: 11-17-2011, 03:16 PM
  3. Project Scuttle - 4DOF Hexapod
    By blobbington in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 08-16-2010, 01:24 PM
  4. Phoniex Hexapod Kit For Sale
    By Quantum in forum Garage Sale
    Replies: 3
    Last Post: 01-20-2010, 03:54 PM
  5. Question(s) Aluminium Thickness
    By sam in forum Mechanics / Construction
    Replies: 11
    Last Post: 09-24-2008, 01:48 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •