Page 1 of 2 12 LastLast
Results 1 to 10 of 14

Thread: Mech Warfare at Sea

  1. #1
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    45

    Question Mech Warfare at Sea

    Surely some of the mech games had water units! I wonder if it would be possible to do a version of Mech Warfare for water "units".

  2. #2

    Re: Mech Warfare at Sea

    That exists. They had "naval" boat battles at Maker Faire.
    The ships are built out of Balsa wood, and the cannons fire steel balls, and actually punch holes in the enemy ships.
    The electronics are all coated so they withstand immersion.

  3. #3
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    45

    Re: Mech Warfare at Sea

    What I mean is not the boats themselves shooting, but the mech being on top of the boat shooting. A lander at sea for example. The boats would be piloted, of couse, but the mechs would have the guns and scoring plates. It would add a level of challenge and open up event location possibilities.
    Last edited by ArduTank; 08-19-2012 at 09:49 PM.

  4. #4
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    56

    Re: Mech Warfare at Sea

    You planning on supplying a tank and storing it? Logistically speaking MW at sea would a nightmare.

  5. #5

    Re: Mech Warfare at Sea

    Logistically speaking MW at sea would a nightmare.
    San Mateo Fairgrounds has a small pool, which was used for the naval battles.
    But I think the intersection between boat builders AND mech builders would be ... small.

  6. #6
    Join Date
    Feb 2012
    Location
    Sydney, Australia
    Posts
    364
    Rep Power
    40

    Re: Mech Warfare at Sea

    Logistics aside, I'd prefer to keep my robots away from water if possible. For a purpose designed boat at least there's a good chance of waterproofing things, but with a legged robot standing on a boat (in particular, with the servos exposed), I'd rather not chance it.

  7. #7
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    45

    Re: Mech Warfare at Sea

    You don't absolutely need a tank. All you need to run it on would be a pond, resivoir,etc, with some float lines to cordone off the area of the arena in the water. And bots don't get splashed if you build the boat with stability and payload in mind, and you can put some short(1"-2") edges on the main deck so the mech doesn't step over. I built a boat that could be scaled to fit the size of a bot's base(distance between feet) that holds a minimum of 10 pounds while needing to be scaled up to hold a quad.

  8. #8
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    45

    Re: Mech Warfare at Sea

    Main Idea of this is, it would be a good idea to have more locations for Mech Warfare. Like with me, I'm hesitant to go because of the cost, and mainly, the closest location is West Virginia.

  9. #9
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    47

    Re: Mech Warfare at Sea

    I'm sure people would appreciate all the BB's we'd dump in the water...

    You also need to protect viewers. And viewers like to be close by so they can actually see... so you can't just put the boats or whatever way off shore.

    Mechs can easily get pushed and tipped over a 1-2" edge, too. And is this one boat or multiple boats? How is transporting these boats cost effective, either?

  10. #10
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    45

    Re: Mech Warfare at Sea

    Quote Originally Posted by ArduTank View Post
    Main Idea of this is, it would be a good idea to have more locations for Mech Warfare. Like with me, I'm hesitant to go because of the cost, and mainly, the closest location is West Virginia.
    This is the ONLY reason I posted this thread. I was giving an Idea that would open up locations for the event. If the event was in more places, you'd probably get more participation.

    P.S. It was multiple boats.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Mech Warfare Turret
    By elaughlin in forum Project Showcase
    Replies: 36
    Last Post: 04-23-2013, 11:28 AM
  2. Interesting Mech Warfare meets Futurised Warfare I hope this is the right place to post.
    By Nadespammer in forum Robotics General Discussion
    Replies: 0
    Last Post: 11-10-2011, 08:38 AM
  3. Mech Warfare gun
    By ahaupt in forum Mech Warfare
    Replies: 7
    Last Post: 02-09-2011, 06:19 PM
  4. Radar for Mech Warfare?
    By mannyr7 in forum Mech Warfare
    Replies: 40
    Last Post: 05-11-2010, 01:40 AM
  5. Autonomy And Mech-Warfare
    By JonHylands in forum Mech Warfare
    Replies: 24
    Last Post: 01-07-2009, 07:35 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •