Results 1 to 3 of 3

Thread: 4S 14.8v lipo battery is charging to 16.5v??

  1. #1
    Join Date
    Sep 2012
    Location
    Alameda, CA
    Posts
    31
    Rep Power
    24

    4S 14.8v lipo battery is charging to 16.5v??

    Hey everyone!

    Quick noob question, I bought a LiPo battery and charger right here from Trossen and I was wondering if it's normal that my 14.8v 4S battery charged to 16.5v when using the balance charging?

    Here are the battery and charger I'm using:

    14.8V 2000mAh Pro Lite Military Spec LiPo Battery
    Imax B6 Multi-Function LiPo Balance Charger

    I'm using a Dynamixel MX-28T servo which is rated for 14.8v, I imagine running 16.5v would be very bad for it right?

    -Alonso

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: 4S 14.8v lipo battery is charging to 16.5v??

    General rule for Lithium chemistry batteries: The max charge voltage of a cell is ~0.5V higher than the nominal voltage, and the max discharge voltage of a cell is ~0.5V lower than the nominal voltage. Most LiPo/Lion cells are 3.7V nominal (4.2V max and 3.2V min), so a 4S pack should go up to 4*4.2V = 16.8V at full charge and go down to no less than 4*3.2V = 12.8V at full discharge. You absolutely must not permit the battery voltage to drop below the lower limit or the cell will be permanently damaged (the charger should prevent the voltage going too high during the charge cycle).

    There was a recent post here about using a 4S pack with MX-series dynamixels and the individual followed up at the Robotis Q&A. Apparently the Nimbro-OP (DARwIn-OP derivative/upgrade) uses a 4S pack safely, but the firmware of the MX-series servos has the default highest voltage limit set to 16V so will produce over-voltage errors until the pack voltage drops a bit. The support site claims the range of valid values for the voltage limit is 50 to 250, so it should be possible to change it and prevent the error.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: 4S 14.8v lipo battery is charging to 16.5v??

    Also, if you want your packs to last longer, don't charge over 4.05V, and don't discharge below 3.35V. This is, AFAICT, what electric cars do to get 10 years projected lifetime with daily use of the batteries. Note that most chargers will just cut off at 4.2V, which is the "safety threshold," rather than the 4.05V limit, so you may have to roll your own if you want best lifetime. Or go with a longer-life chemistry, like LiFePO4.

    Also, the curve for "voltage vs charge" is not linear at all -- at the very left (low charge) it rises quickly from 3.2V to 3.5-3.6V, and on the right, it takes a long time before it rises above 3.8V/3.9V and shoots towards 4.2V. This makes a "gas gauge" for a LiPo battery pretty hard to build, but it also means you could just use the 3.4V - 4.0V range as your design limit, and not use the extreme values, because the amount of charge (running time) represented by those areas is actually pretty small.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Charging computer NIHM battery pack
    By Xalu in forum Power
    Replies: 5
    Last Post: 11-19-2011, 06:59 AM
  2. Question(s) Monitoring LiPo battery while it's in use.
    By Stobs in forum Power
    Replies: 4
    Last Post: 10-04-2011, 10:01 AM
  3. Question(s) LiPo Battery cut off safety?
    By Pinter75 in forum Power
    Replies: 11
    Last Post: 03-15-2009, 04:52 PM
  4. charging and battery system
    By asbrandsson in forum Robot Computers
    Replies: 1
    Last Post: 01-29-2008, 04:54 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •