The cool thing is that it is free and it is a open hardware and software project!!!
http://mike-ibioloid.blogspot.com/20...s-now-out.html
The cool thing is that it is free and it is a open hardware and software project!!!
http://mike-ibioloid.blogspot.com/20...s-now-out.html
I also saw this earlier, Lots of possibilites.
http://mike-ibioloid.blogspot.com/2012/10/cm-900.html Just uploaded pictures!
I just bought one of the new CM-900 version 1.01 boards at the Bay Area Maker Farie.
http://mike-ibioloid.blogspot.com/20...o-control.html
They had a buy one get one free deal at the faire!!
The Specs for the CM-9.04 New Open Source Servo Control Board from Robotis have just been released.
http://mike-ibioloid.blogspot.com/20...en-source.html
Only 10 dollars USD now!!!!!
CM-9.04 CM-900 CPU STM32F103CB (ARM Cortex-M3) STM32F103C8 (ARM Cortex-M3) Op Voltage 5V~16V( USB 5V, DXL 12V, 7.4V) 5V~35V( USB 5V, DXL 12V, 7.4V) I/O GPIO 28 GPIO 32 Timer 8 8 Analog In(ADC) 10(12bit) 10(12bit) Analog Out(DAC) X X Flash 128 Kbytes 64 Kbytes SRAM 20 Kbytes 20 Kbytes Clock 72Mhz(9 X 8Mhz) 72Mhz(9 X 8Mhz) USB 1(2.0 FS) 1(2.0 FS) CAN 1 1 USART 3 3 SPI 2 2 I2C(TWI) 2 2 Debug JTAG & SWD JTAG & SWD DMA 7ch 7ch 3 Pin TTL 4(AX12 Compatible 3Pin) 2 4 Pin RS485 X 2 Mini 3Pin TTL 4(AX12 Compatible 3Pin) 1 External ADC Ref YES NO DC Jack NO YES S/W ROBOTIS CM9 ROBOTIS CM9 SIZE 27mm X 66.5 mm 60mm X 54 mm Price Around 10$ Around 20$
The limited voltage range of the 9.04 means you can't run it on 16.8V maximum output 4S LiPos?
I guess you could use a separate 5V converter to power the board, if it allows servo power to be separate?
What servos are you running with that setup?
MX-64. They are rated for 4S LiPo according to Robotis support.
There are currently 1 users browsing this thread. (0 members and 1 guests)
Bookmarks