Page 2 of 2 FirstFirst 12
Results 11 to 13 of 13

Thread: Another three-servo walker

  1. #11
    Join Date
    Feb 2012
    Location
    Sydney, Australia
    Posts
    364
    Rep Power
    35

    Re: Another three-servo walker

    Eww...

    I've heard of using ferric chloride to get rid of broken taps in titanium (eats at Ti much slower than steel), perhaps something similar could be done here? Unsure on specifics for aluminium though.

  2. #12

    Re: Another three-servo walker

    Right now, I'm running with three screws and nothing in that fourth hole. I'll try not to re-do that mistake if I ever make "finish" parts :-)

    I also added a webcam now (a Microsoft LifeCam HD.) It provides the images over the same WiFi as the remote control, and it works great!
    Unfortunately I have to use tiny images (432x240) to fit each MJPEG image in a UDP datagram (< 64kB) but it still works alright. I may just add multiple-datagram support to my protocol and rely on IP fragmentation; it ought to be OK.

    It's also surprisingly cool to be able to "ssh" into a command line on a robot that's walking around the kitchen on remote control and sending images back alread. Gives you that "robot overlord" feeling :-)

    Next up: pan/tilt support, and a real mount for all the gear. After that, gun. In parallel, improve the gait to use a non-interference solver to move the legs at all times. After that: hope Trossen starts selling the targeting system again, and start practicing! (Actually, this is for my son. So, get him to start practicing!)

  3. #13
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    42

    Re: Another three-servo walker

    I won't lie, if I had a robot that I could SSH into (alas I'm an 8bit nub), I'd run radiation transport calculations on the bot while also having it walk around.

    I'll comment more about the bot when I see actual pictures

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Bioloid Biped Walker
    By Noog in forum Humanoids, Walkers & Crawlers
    Replies: 6
    Last Post: 12-05-2011, 01:37 AM
  2. Rover or walker?
    By SteamAutomaton in forum Robotics General Discussion
    Replies: 8
    Last Post: 09-16-2009, 07:59 PM
  3. Beam walker
    By Grand Robot Master in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 04-16-2009, 11:18 PM
  4. Beam walker
    By Grand Robot Master in forum Robotics General Discussion
    Replies: 0
    Last Post: 04-16-2009, 10:07 PM
  5. Knuckle Walker?
    By rudukai13 in forum Mech Warfare
    Replies: 17
    Last Post: 07-29-2008, 09:46 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •