Results 1 to 3 of 3

Thread: Understanding accelerometrs data

  1. Understanding accelerometrs data

    Hi,

    My name is Tomer and I like to build robots and automated machines as a hobby.
    Lately I started working with digital accelerometers and Gyros.

    I saw the thread about the L3G4200D Gyro and it was very helpful.
    I bought this gyro and several other accelerometrs from ST.

    my question is a general one that concern to all digital accelerometers (at least those from ST).
    I am having problem translating the data I receive from them. I have a few questions:
    1. for the simplest example: I tried to convert the data of an 8 bit accelerometer based on 2 application notes: AN2988 and AN2989, in both of them there is an example of the acceleration value and the value received in the register (section 2.4.2).
    a. How do I convert the number from the register into g?
    b. since they are both 8 bits, why are the values not the same?

    Links:
    AN2988: http://www.st.com/internet/com/TECHN...CD00236138.pdf
    AN2989: http://www.st.com/internet/com/TECHN...CD00236147.pdf

    2. when using a 12 bit accelerometer I receive the data in 2 registers, that is 16 bits. when I combine them, should I ignore bits 15-12 or 0-3 (working in the default mode of Little Endian) can you please show me how to convert the register values into acceleration values in AN3308 section 3.2.3.
    http://www.st.com/internet/com/TECHN...CD00290365.pdf


    Thanks,
    Tomer.

  2. #2

    Re: Understanding accelerometrs data

    since they are both 8 bits, why are the values not the same?
    Because it measures acceleration in two different directions. Those directions should be spelled out in the data sheet, and are relative to the chip itself. Btw: most modern accelerometers measure 3 cardinal directions. Also, the G force of the Earth will be part of the reading, so whatever part of your axes point downward will see that.

    How do I convert the number from the register into g?
    The data sheet should tell you, but generally, if you know that the range is [-X to +X] then typically an unsigned value will map 0 to -X, and 255 to +X, and a signed value will map -127 (or -128) to -X and 127 to X. You can then recover the "g" reading by doing simple scaling. There may be calibration/offsets you want to add, too.

  3. Re: Understanding accelerometrs data

    [QUOTE=jwatte;54156]Because it measures acceleration in two different directions. Those directions should be spelled out in the data sheet, and are relative to the chip itself. Btw: most modern accelerometers measure 3 cardinal directions. Also, the G force of the Earth will be part of the reading, so whatever part of your axes point downward will see that.

    Thanks for the answer.

    Actually, this is because the sensitivity is different between the 2. silly of me not to notice that before.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Understanding URDF files and rviz in ROS
    By Pi Robot in forum ROS - Robot Operating System
    Replies: 9
    Last Post: 10-24-2010, 09:28 AM
  2. Understanding a 3-XBEE network?
    By Pi Robot in forum Arbotix, Microcontrollers, Arduino
    Replies: 11
    Last Post: 09-09-2010, 03:45 PM
  3. Bioloid Understanding the Premium Gyro Sensor Module
    By Zlosk in forum Humanoids, Walkers & Crawlers
    Replies: 13
    Last Post: 04-25-2010, 02:14 PM
  4. Help understanding a diagram
    By Resilient in forum Robotics General Discussion
    Replies: 3
    Last Post: 03-30-2009, 12:27 AM
  5. Question(s) Getting Data In !
    By flybythemoon in forum Arbotix, Microcontrollers, Arduino
    Replies: 8
    Last Post: 06-20-2008, 07:37 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •