Results 1 to 2 of 2

Thread: Stilgar's bot called RED

  1. #1

    Stilgar's bot called RED

    Hey guys/gales,


    After many years of doing other things I decided to get back to robotics. I have many Ideas and projects in mind but thought I should start small to see how much I remember. So here I present my bot named RED.

    What he will do is run free until he comes to a obstacle, Then will look to both sides with his sensor turret to find a clear path. He will decide where the clear path is, turn in that direction, and go on his marry way until the next obstacle.

    Click image for larger version. 

Name:	Red 1.jpg 
Views:	516 
Size:	35.5 KB 
ID:	4369Click image for larger version. 

Name:	Red 2.jpg 
Views:	517 
Size:	24.3 KB 
ID:	4370Click image for larger version. 

Name:	Red 3.jpg 
Views:	535 
Size:	25.5 KB 
ID:	4371Click image for larger version. 

Name:	Red 4.jpg 
Views:	497 
Size:	24.5 KB 
ID:	4372


    I am using a Parallax Propeller controller, running at 8Mhz, mounted on a custom board. He will have a Sharp GP2Y0A2YK IR Infrared Range Sensor in the turret to detect obstacles. The chassis is a Re-purposed spy gear ATV 360. I have 2, (one of the transmitters was damaged). He tips the scale at about 2 pounds (30 Oz). Runs on 9 Volts by 6 AA cells. The body and turret was handmade in sheet styrene plastic.

    Some more pics of the custom control board with the parallax chip, and the current inside of RED. The dual H-bridge motor control is currently being built. The sensor is on order.

    Click image for larger version. 

Name:	Red brain.jpg 
Views:	516 
Size:	21.5 KB 
ID:	4374Click image for larger version. 

Name:	Red current inside.jpg 
Views:	518 
Size:	32.9 KB 
ID:	4373






    For those that never seen a spy gear ATV 360, here is a pic, also shown is the original receiver board.

    Click image for larger version. 

Name:	spy_video_circuit_board.jpg 
Views:	494 
Size:	124.7 KB 
ID:	4375Click image for larger version. 

Name:	ZHRfXwnw6noraxdwBRkrFfCNo1_400.jpg 
Views:	513 
Size:	16.6 KB 
ID:	4376

    More to come,
    Stilgar
    Projects: Design, build, use, modify, recycle, tweak, lather, rinse, repeat

  2. #2

    Re: Stilgar's bot called RED

    Little update. RED is running, a vid to test movement. I discovered my H-bridge has a problem, I'am not getting the full 9 volts to the motors. No sensor installed, just running program sequence.

    Projects: Design, build, use, modify, recycle, tweak, lather, rinse, repeat

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. News/Announcement New german robotics podcast called 'Roboiklabor'
    By robotiklabor in forum Robotics General Discussion
    Replies: 0
    Last Post: 04-25-2012, 07:27 AM
  2. What's this part of the faucet handle called?
    By spiffwilkie in forum Off Topic
    Replies: 2
    Last Post: 09-16-2008, 12:08 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •