Results 1 to 6 of 6

Thread: About to give up on the Raspberry Pi

  1. #1

    About to give up on the Raspberry Pi

    I've been trying to make my quad walk on its own using a Raspberry Pi for control, and a ATmega32u4 for the low-level servo control, talking USB.
    The ATmega32u4 and the control program works great on regular Intel hardware with Linux. However, on the RPi, I've been getting strange, intermittent cases of USB just dropping off the Earth.
    Now, I've found a thread on the RPi forums about the RPi having USB hardware bugs that the software tries to work around, but may not be able to do. That's... a shame! It's a nice, small form factor with reasonable power. The next "step up" would be a BeagleBone, with approximately the same amount of power but a higher price point, and unknown USB capabilities.

    Then I found this:
    http://www.zotacusa.com/zbox-nano-xs-ad11-plus.html

    1
    05x105x45 cm, full x86 compatibility (AMD,) solid chipset. I'm in love!

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    282

    Re: About to give up on the Raspberry Pi

    I do believe that is what the NimbRo-OP uses with its 4S battery instead of a fit-pc2i-sbc. The E-350 in my pc works quite nicely and the slower C-60 in my netbook can almost play 1080p movies smoothly (have not tried the restricted drivers). Unfortunately, ATI GPU processing is not as widely supported/popular as NVIDIA CUDA.

    edit: bleh, the fglrx drivers suck something awful.
    Last edited by tician; 01-13-2013 at 05:21 PM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: About to give up on the Raspberry Pi

    The gpu would actually go unused. Unless I use it for development, too!

  4. #4
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    132

    Re: About to give up on the Raspberry Pi

    I've actually been looking at these as well. The AMD-based Zotacs look to be quite a bit less power hungry and expensive than the Intel NUC. One thing to keep in mind is that there are actually 3-generations available, the AD10, AD11, AD12. The AD11 for whatever reason uses a USB-based Wifi (unlike the mini-PCIe used in the 10/12 generation).

    -Fergs

  5. #5

    Re: About to give up on the Raspberry Pi

    Ad12? Didn't see that one.
    Is it smaller than the 11?

  6. #6

    Re: About to give up on the Raspberry Pi

    No, it's bigger. So ad11 it is! And it looks like you could pull the circuit board out if you wanted a custom enclosure.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Raspberry Pi
    By Robonaut in forum Robot Computers
    Replies: 20
    Last Post: 07-07-2013, 10:46 AM
  2. raspberry pi for robotics? ROS? Rover bot
    By SuperMiguel in forum Software and Programming
    Replies: 6
    Last Post: 05-23-2013, 05:43 PM
  3. Just For Fun My Raspberry PI
    By rebel in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 12-31-2012, 05:57 PM
  4. Raspberry Pi WiFi questions
    By ArduTank in forum Robot Computers
    Replies: 1
    Last Post: 12-26-2012, 03:45 PM
  5. Bioloid AX-12 servo give up its torque
    By Roman Burdakov in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 01-03-2012, 10:19 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •