Trossen Force Sensor  Top Banner
+ Reply to Thread
Page 2 of 2 FirstFirst 12
Results 11 to 15 of 15

Thread: UK Mechwarfare / Lynxmotion

  1. #11

    Re: UK Mechwarfare / Lynxmotion

    $2,000 that's not bad when you consider how much people spend on the combots.
    I'm at 3x that by now. My wife's comment when she totalled up the bill: "You'd /better/ win!"
    No pressure...

  2. #12

    Re: UK Mechwarfare / Lynxmotion

    it seems we only have the combots over here which I find a bit dull
    If you have the available time, perhaps you could organize something yourself? Tie into some existing robot meet, and announce and market the event. Start out with just an open league, to let people start easily with hexes and tanks and whatnot. Aim for four or five contestants from across Europe, and spend *all* your time evangelizing to get competitors.

    Take lots of video and photos when you actually hold the event, and use for marketing the next year. Repeat :-)
    If you can get a club or some friends to "seed" the competition by committing a 'bot or two, you have a much better chance of getting bootstrapped, too.

    Whether you could/should use the name "mech warfare" I have no idea -- probably a good idea to check out before you get serious about this, if you do.

  3. #13
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    828
    Images
    20
    Rep Power
    38

    Re: UK Mechwarfare / Lynxmotion

    I've always been rather fond of the dirt cheap and easy target sensors used at a mechwarfare-type event several years ago in Japan. Basically, a little wire cube about 2" on a side covered in aluminium foil with a Cadmium Sulfide ambient light sensor in the bottom of it (probably less than $10 for everything). The more holes the airsoft pellets punch into the foil, the greater the incident light. Once it reaches some limit, then the bot is deemed dead. You could even connect the sensor and cheap microcontroller to a biggish MOSFET or SSR at the battery to kill the bot's power.

    edit: upon further pondering, the big box of ~60mm square solar cells under my bed would probably be a better choice than an itty-bitty CdS photocell.
    Last edited by tician; 01-25-2013 at 12:27 AM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"

  4. Re: UK Mechwarfare / Lynxmotion

    Thanks Jwatte, I was thinking this myself. I wouldn't be able to do it right now, clearly takes a lot of time and effort, but perhaps one day in the near future. I've already had a friend offer to help build an arena/scenery. I would try and make it more open to start with, allowing hex's and tanks, though tanks may have to be in a separate class. Heck, perhaps one day we can include quad coptors? Something like the AR.Parrot drone with a bb gun under it flying around the city scape.

    Tician, yeah I've seen what the Japanese have done, very ingenious and I like the idea of the bots powering down once their hit points run out.

    Do you guys get to see your hit points or do the organisers see them? You could overlay them using something like a Propeller backpack so you have a HUD on your screen. Possibly also have two giant screens at the arena showing this footage as well for the audience?

  5. #15
    Join Date
    Sep 2009
    Location
    Baumholder, GE
    Posts
    279
    Images
    51
    Rep Power
    19

    Re: UK Mechwarfare / Lynxmotion

    My next robot, keep in mind it is a Biped, has already gone over $4K. One thing I will tell you, going cheap does not work for these robots

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. MechWarfare entry HD2
    By Janis in forum Mech Warfare
    Replies: 17
    Last Post: 04-19-2013, 06:32 AM
  2. News/Announcement Win a Lynxmotion A-Pod!
    By Robot Dude in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 04-16-2012, 09:16 AM
  3. MechWarfare => Armored Core V
    By Fanatic in forum Mech Warfare
    Replies: 1
    Last Post: 06-16-2011, 11:04 AM
  4. Replies: 4
    Last Post: 09-19-2010, 10:18 AM
  5. Mechwarfare National anthem
    By Promagic in forum Mech Warfare
    Replies: 8
    Last Post: 04-21-2009, 06:29 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts