Results 1 to 3 of 3

Thread: ArbotiX with LabVIEW: Low-level ArbotiX Commands?

  1. Question ArbotiX with LabVIEW: Low-level ArbotiX Commands?

    Hi,

    I need to use LabVIEW to interact with an ArbotiX Robocontroller. I've surfed for hours trying to find the basic low-level commands for the ArbotiX, but I always get sent to Python scripts or some other library. I have no desire to try to interface LabVIEW to Python scripts. I did wade through some of the Python scripts and controlling the ArbotiX appears to be as simple as sending commands down a COM port (which LabVIEW does very well).

    Are the *basic* ArbotiX commands and syntaxes documented somewhere? I'm controlling a PhantomX Reactor (AX-12A servos).

    Thanks.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: ArbotiX with LabVIEW: Low-level ArbotiX Commands?

    The ATmega644p used in the arbotix has two UART interfaces. One UART is used for the dynamixel bus and the other for communicating with the pc and/or wireless controller. If you check the arbotix code repo (should be linked on the trossen shop pages), you should find the example sketches and the commands they accept. If they do not suit your needs, you can program the arbotix to do just about anything you want and using any message format you want as long as it is sent over the Xbee/FTDI link at a reasonable baudrate. 38400/57600 bps is about the max you can reliably get with Xbee, but USB/FTDI can easily go to 1Mbps without any data loss.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. Re: ArbotiX with LabVIEW: Low-level ArbotiX Commands?

    The code repo is obviously very complete - it's a matter of cobbling the pieces I need which isn't terribly difficult, but it is time-consuming. I'm in the process of pulling together a reasonable driver I can call from LabView. If it seems innovative or broadly applicable, I'll post it and the VIs I use to call it.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Arbotix 0.5.0
    By lnxfergy in forum ROS - Robot Operating System
    Replies: 17
    Last Post: 08-13-2012, 10:51 AM
  2. Question(s) MX-28 and Arbotix
    By jakerockwell in forum Software and Programming
    Replies: 6
    Last Post: 07-15-2012, 08:00 AM
  3. Question(s) EX-106 servos with arbotix
    By tduv in forum Project Showcase
    Replies: 0
    Last Post: 05-26-2012, 12:50 PM
  4. Question(s) Arbotix & I2C
    By sarendt in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 05-14-2012, 11:41 AM
  5. Question(s) Labview Microcontrollers
    By PseudoNym00 in forum Robot Computers
    Replies: 7
    Last Post: 11-14-2008, 11:59 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •