Results 1 to 6 of 6

Thread: lipo battery for irobot

  1. lipo battery for irobot

    Has anyone tried to disconnect the original charging circuitry in irobot and succeeded to power on the irobot with a lipo battery??

  2. #2
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

    Re: lipo battery for irobot

    I think it's 14v so I suppose a 4cell lipo would work. Though as you stated do NOT try and charge it with the internal charger. I suppose the next question is why do you want to switch? Weight?

  3. #3
    Join Date
    Jun 2010
    Location
    Australia
    Posts
    161
    Rep Power
    35

    Re: lipo battery for irobot

    I plugged the thread title into Google & the fourth one on the list was;
    www.youtube.com/watch?v=jHpg6Zz8XVE

    I can't view youtube clips at this computer, but i'm guessing they have done it successfully.
    As Kevin0 suggests above, the charging could be an issue. Good luck though!

  4. Re: lipo battery for irobot

    @Kevin0, I need to increase its running time,because the OEM rechargable NIMH has a running time of only 1.5 hour and also lipo has a better perfomance.
    Can you recommend me a name for lipo battery with good life time , low weight and size?

  5. #5
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

    Re: lipo battery for irobot

    http://thunderpowerrc.com/ Is what I use for all my projects. Look through the data sheets and find a 4 cell that has measurments that fit in the compartment the original batterys used to sit in.

  6. Re: lipo battery for irobot

    I use tigers lipo batteries for rc choppers. They come in different sizes, voltage etc. Make sure you use a balanced charger if your using multiple cells.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) 4S 14.8v lipo battery is charging to 16.5v??
    By alonso in forum Power
    Replies: 2
    Last Post: 10-14-2012, 11:23 PM
  2. Question(s) Monitoring LiPo battery while it's in use.
    By Stobs in forum Power
    Replies: 4
    Last Post: 10-04-2011, 10:01 AM
  3. For Sale: 5S 18.5v 4000mAh LiPo 25C Battery
    By DresnerRobotics in forum Garage Sale
    Replies: 1
    Last Post: 07-23-2009, 11:07 AM
  4. Question(s) LiPo Battery cut off safety?
    By Pinter75 in forum Power
    Replies: 11
    Last Post: 03-15-2009, 04:52 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •