Results 1 to 7 of 7

Thread: Dynamixel AX-12A not responding

  1. Dynamixel AX-12A not responding

    Some of my AX-12 servo's changed there id. After reading related posts (seemed to be a known problem) i tried to reset the ID. I had just 1 servo connected to my ArbotiX Robocontroller i send a "set id" (ax12SetRegister AX_ID) command.
    Now my servo is not responding at all. (Checked id 0-255 on a rang of baud rates)

    Is there a way to reset the ax-12 (with a ArbotiX Robocontroller) I don't own a USB2Dynamixel.

    Hope somebody can help me.

    Martin

  2. #2

    Re: Dynamixel AX-12A not responding

    If you're seriously playing with these kinds of servos, getting one is a pretty important investment. I know of no other way to reset/recover the firmware than using an USB2Dynamixel.
    Maybe some of the Robotis controllers can emulate the USB2Dynamixel function? Anyone know?

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,297
    Images
    27
    Rep Power
    278

    Re: Dynamixel AX-12A not responding

    Quote Originally Posted by jwatte View Post
    Maybe some of the Robotis controllers can emulate the USB2Dynamixel function? Anyone know?
    You should be able to program a CM-510/530/700 using embedded-c to simply pass everything between the USB UART and the dxl UART, but it's not possible using RoboPlus Task. An arbotix would probably be able to do it as well. The USB2Dynamixel is pretty much just an FT232RL USBtoUART with a bit of full-duplex to half-duplex logic for the 'ttl' dynamixel bus.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh
    more bleh

  4. #4
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

    Re: Dynamixel AX-12A not responding

    Have you tried https://github.com/KurtE/AX12_Test ? It has a few commands that are using the broadcast id. If they respond to that it might be something simple that doesn't require a full reset/restore.

  5. Re: Dynamixel AX-12A not responding

    Thanks all. Guess my next order will be the USB2Dynamixel.

  6. #6
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    42

    Re: Dynamixel AX-12A not responding

    Another option is the USB2AX. http://www.seeedstudio.com/depot/usb2ax-p-1349.html

    You still have to provide power to the servos, but I use a custom perf-board + power supply setup for that.

  7. #7
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

    Re: Dynamixel AX-12A not responding

    I just bought one of those! I'm using the usb2dynamixel right now with my raspberry pi. Looking forward to switching it out with one of those.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Dynamixel MX-64 on 4s Lipo
    By r691175002 in forum Robotics General Discussion
    Replies: 4
    Last Post: 10-04-2012, 10:31 PM
  2. News/Announcement Dynamixel MX-64 and MX-106
    By pauljurczak in forum DYNAMIXEL & Robot Actuators
    Replies: 22
    Last Post: 05-26-2012, 07:51 PM
  3. dynamixel servors AX-12
    By gwntd in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 04-27-2012, 10:32 PM
  4. Dynamixel vs. Hi-Tec
    By mblackwolf in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 11-26-2011, 05:56 PM
  5. Question(s) Dynamixel
    By Grand Robot Master in forum DYNAMIXEL & Robot Actuators
    Replies: 8
    Last Post: 04-26-2009, 03:43 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •