Results 1 to 3 of 3

Thread: link two ax12 servos

  1. link two ax12 servos

    I have searched the forum but I can't find the answer.
    Is there a way to link two ax12 servos so that they move together using dynamixel programing?
    Thanks
    Bob

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: link two ax12 servos

    Just send them the same goal positions (very slight delay between start of motion), or send a sync-write packet identifying the servos you want and give them the same goal/speed values (synchronized start of motion). RoboPlus task cannot use sync-write, but it can easily use independent packets. Arbotix/Arduino/Maple/CM-900, embedded-c (CM-510/530/700), and PC with USB2Dynamixel or USB2AX can easily use sync-write.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. Re: link two ax12 servos

    Thanks

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Discussion Link Cell Phone to Microcontroller
    By liam.tr in forum Robotics General Discussion
    Replies: 4
    Last Post: 04-01-2010, 02:05 PM
  2. alright here's the link
    By csdude in forum Rovers
    Replies: 5
    Last Post: 02-12-2010, 01:13 AM
  3. Discussion AX12 servos
    By 4mem8 in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 12-27-2008, 04:45 AM
  4. Link to linkages
    By kdwyer in forum Mechanics / Construction
    Replies: 0
    Last Post: 12-28-2007, 05:33 PM
  5. Phidgets API Download Link
    By claymore1977 in forum Software and Programming
    Replies: 3
    Last Post: 11-24-2007, 11:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •