Results 1 to 5 of 5

Thread: The D-Link DCS930L Camera and you

  1. #1
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    44

    The D-Link DCS930L Camera and you

    I got tired of digging into the middle of another thread to check info on the DLink DCS930L wireless camera, so here is a thread combining all the relevant information for this camera.

    Previous threads
    - DLink stuff on pages 3 and beyond

    Camera internals/details
    To take the camera apart, pry off the front white panel. The grey trim is part of the back half of the case.

    For Pictures, See mannyr7's post.

    The included power supply is 5V @ 1.2A. Uses a standard barrel connection (same as Trendnet cameras, for example)

    Weight is 59 grams, case and all.

    The camera board includes an auxilliary antenna connector. It is not known if this actually is used if an antenna is attached.

    CAD Model and integrating the board into your design
    I whipped this up a while ago. See the attached D-Link DCS930L board.zip (.igs format; camera internals only)

    The method that several mechs use for mounting the camera board is to encase it in several layers of (lasercut) plastic. Specifically you need a piece cut from .125" material and a piece from 3/32" material; These will surround the camera, and then you need a front and back plate to hold it in place. Illustration (click to embiggen):
    Click image for larger version. 

Name:	twitchcamcadannotated.jpg 
Views:	3064 
Size:	55.4 KB 
ID:	4626

    Viewing the D-Link camera
    Two options:

    1. Use the in-browser viewer, which is reached by putting the IP address of the camera in the URL bar. (Bizarre: an emulator of what this looks like)
    2. Use Python to capture the video stream. Upgrayd's repo on Github will do this for you. (specifically server/MWCam.py)

    For reference, Python takes advantage of

    Quote Originally Posted by mannyr7
    A little searching in the D-Link forum produced these links:

    http://<camera ip>/video/mjpg.cgi

    http://<camera ip>/image/jpeg.cgi
    http://<camera ip>/image/jpeg.cgi?profileid=1

    Paste these in your browser or imaging software of choice to view streams or stills devoid of the D-Link GUI.
    Bonus: Upgrayd's Python script includes code that talks to the scoring server in MW, so you get the current scores overlaid.
    Click image for larger version. 

Name:	mwcamdlink.png 
Views:	3281 
Size:	398.9 KB 
ID:	4624

    Firmware
    DLink has 7 or so versions of firmware for the camera. These can be downloaded from here.

    If you are using Python to stream the footage, I have found that some of these firmware versions result in huge lag and ~1FPS, while the rest are fine... The WORKING versions of the firmware for me are 1.03, 1.04, 1.06. 5 7 8 all are bad, and I did not test 0 and 2. There may be other advantages to different firmwares, I only tested framerate. Also, some of the newer firmwares seem to not work properly with older versions of DLink's camera setup software. These installers are also available at the above link.

    Bricked?
    Try holding down the reset button, powering it on, and keep holding the rest button down for ~10s. Then hook it up via ethernet and look for IP address 192.168.0.20 or 192.168.0.5 in the browser. (Your computer must be on the 192.168.0.x subnet) More info in this thread.

    Issues?
    I have had issues with mine resetting itself: it fails to connect to wifi, and then the DLink setup software finds the camera and reports the camera as not configured. I have a spare ordered for this reason...
    Attached Files Attached Files

  2. Re: The D-Link DCS930L Camera and you

    Hi, I'm new and have been lurking the crap out of these forums the last 2-3 weeks. Posts like this make me smile. Concise, condensed, with references and a CAD model to boot. Thanks for the solid info Gertlex.

  3. #3
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    44

    Re: The D-Link DCS930L Camera and you

    If you still want to grab one of these cameras, on sale through tomorrow for a nice price:

  4. #4
    Join Date
    Aug 2009
    Location
    Raleigh, NC
    Posts
    58
    Images
    39
    Rep Power
    36

    Re: The D-Link DCS930L Camera and you

    So I've used the 930L quite a bit for a teleoperated robot over the past year, and I can definitely speak to the pros and cons of this camera.

    To give a little background, I've put the camera on two teloperated robots, one with tank treads and the other with omniwheels. The control for the robots were over Xbees, so the only wifi traffic was the camera. For viewing, I've used Upgrayd's code and used the included software with the camera.

    Pros:
    • Lightweight
    • Low power consumption
    • 640x480
    • Great visibility (when in good signal range)
    • 2.4/5.8 Ghz
    Cons:
    • Seems to drop connection when moderately far from router
    • Randomly has low framerates
    • Hard to attach to something other than the stand (unless you rip the post off the back of it, then glue it to something)
    So I would love to say that this camera was awesome and that this is the best one for using with MW, but sadly it isn't. I'm actually rather peeved at the camera, since a team of robotics engineers at NC State university actually lost a competition due to this camera (thanks to a network drop out right before we had to compete).

    I've used two different Linksys routers (WRT54GL and E1200) and I've used both 2.4Ghz and 5.8Ghz for testing. I also used both of the video viewers mentioned above. Long story short, at short distances with a clear line of sight, and not in the presence of other network devices causing interference, this is a great camera. During our competition, I had to place the "command center" behind a black plastic curtain, and my framerates dropped from 30 to 1, just by putting the router behind a curtain. I really do think it's the camera that's the problem, and not the routers.

    Anyway, I hope you all find this useful, and you might want to look into the RF cameras, rather than networked cameras.
    Always outnumbered, never outgunned. Axiom Robotics

  5. #5
    Join Date
    Apr 2013
    Location
    Boston, MA
    Posts
    260
    Images
    11
    Rep Power
    30

    Re: The D-Link DCS930L Camera and you

    Sorry for the OT, but i have to give a Wolfpack shout out! I graduated from ECE in '04. Sorry for the frustrating loss. Sounds like you guys are up to some interesting stuff, though. I wish they had or I had known about that stuff back then.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 61
    Last Post: 04-21-2013, 11:27 PM
  2. link two ax12 servos
    By hawaiibob in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 03-23-2013, 07:33 PM
  3. alright here's the link
    By csdude in forum Rovers
    Replies: 5
    Last Post: 02-12-2010, 01:13 AM
  4. Link to linkages
    By kdwyer in forum Mechanics / Construction
    Replies: 0
    Last Post: 12-28-2007, 05:33 PM
  5. Phidgets API Download Link
    By claymore1977 in forum Software and Programming
    Replies: 3
    Last Post: 11-24-2007, 11:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •