Results 1 to 6 of 6

Thread: Home made Arduino robot - crawler/tank

  1. Home made Arduino robot - crawler/tank

    Just finished the code and I'm finally happy with the performance.
    Most of the parts are bought from ebay, low budget build.



  2. #2

    Re: Home made Arduino robot - crawler/tank

    I think it's cute. The video was very explanatory.

    Any particular reason why you decided to build your own h-bridge instead of buying an off the shelf part?

  3. #3
    Join Date
    Dec 2012
    Posts
    67
    Images
    13
    Rep Power
    32

    Re: Home made Arduino robot - crawler/tank

    Very well made ​​~
    clean and good design.

  4. Re: Home made Arduino robot - crawler/tank

    Quote Originally Posted by CasperH View Post
    I think it's cute. The video was very explanatory.

    Any particular reason why you decided to build your own h-bridge instead of buying an off the shelf part?
    Quote Originally Posted by hwan we View Post
    Very well made ​​~
    clean and good design.
    Thanks guys! The reason i built my own H-bridge is mostly because it's more fun than buying it of the shelf.. And I was afraid the ready-made h-bridges would not handle the current. They are often rated between 1-2 amps, and the one I made can handle up to 10 amps.

  5. #5

    Re: Home made Arduino robot - crawler/tank

    I was afraid the ready-made h-bridges would not handle the current
    Actually, some of those are just intended to provide gate current for big MOSFETs to deal with whatever current you want.
    The reason they need a full amp or more is that powerful MOSFETs need really quite a lot of current very quickly to switch on or off.

    I can't see much of your circuit board; it looks like maybe you're using pull-up resistors to turn on P-channel and off N-channel, and then use a smaller transistor to pull to ground for the inverse? If that's what you're doing, you're current limited on the pull-up resistor value. Looks like maybe 100 Ohms? If so, then I would expect (based on experience!) you can do OK with Arduino-level PWM (400 Hz or so) but if you try to raise the PWM frequency, you'll start blowing the MOSFETs.

  6. Re: Home made Arduino robot - crawler/tank

    Quote Originally Posted by jwatte View Post
    Actually, some of those are just intended to provide gate current for big MOSFETs to deal with whatever current you want.
    The reason they need a full amp or more is that powerful MOSFETs need really quite a lot of current very quickly to switch on or off.

    I can't see much of your circuit board; it looks like maybe you're using pull-up resistors to turn on P-channel and off N-channel, and then use a smaller transistor to pull to ground for the inverse? If that's what you're doing, you're current limited on the pull-up resistor value. Looks like maybe 100 Ohms? If so, then I would expect (based on experience!) you can do OK with Arduino-level PWM (400 Hz or so) but if you try to raise the PWM frequency, you'll start blowing the MOSFETs.
    You've got a point, buying ready-made h-bridge and using a MOSFET would probably be the easiest way. In this H-bridge there are no MOSFETS though, only NPN and PNP -transistors. I dont think the pwm-signal will damage the npn-transistor, but I guess one could make a low-pass filter if it becomes a problem. The high current does not pass through any resistors along the circuit (except the motors themself). It is more or less the same circuit as this and it seems to perform nicely;
    http://wilf.solarbotics.net/PSHbridge/PShbridge.gif

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Just For Fun ToBo (Home-made Toy Robot.. Mini Enthiran... DIY... )
    By WilliesWonderWorld in forum Project Showcase
    Replies: 3
    Last Post: 06-19-2012, 08:29 AM
  2. Choosing input type for home made servo controller
    By tigrlily in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 06-05-2011, 04:23 PM
  3. I-sobot + Arduino interfacing made easy
    By Nelsontheunholy in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 01-21-2010, 04:17 PM
  4. Congratulations! you made it on Robot magazine!
    By Promagic in forum Mech Warfare
    Replies: 10
    Last Post: 01-17-2009, 05:26 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •