Results 1 to 4 of 4

Thread: Would the AX-12W be better then AX-18A for the PhanomX Hexapod MarkII

  1. Would the AX-12W be better then AX-18A for the PhanomX Hexapod MarkII

    I'm looking into getting a hexapod and I came across the AX-12W. Before I was thinking of getting the full kit that comes with the AX-18A, but the AX-12W seems worth looking in to. Seeing as the 18's have 18.3 kg·cm stall torque and the 12W's only have 2.0 kg-cm, would 2 kg-cm be enough to allow the robot to function or would it just stall and overheat? If this has already been asked and answered or anyone has any useful advice that would be great.

    Thanks

  2. #2
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    42

    Re: Would the AX-12W be better then AX-18A for the PhanomX Hexapod MarkII

    It would be too weak, for sure. You're talking a factor of 9 weaker than AX-18As, 7.5 weaker than an AX-12. If I'm wrong, you'd still have no payload capacity whatsoever

    The W servos are for wheeled applications that don't require lots of torque. They aren't for joints in robot arms/limbs.

  3. Re: Would the AX-12W be better then AX-18A for the PhanomX Hexapod MarkII

    Haha I love your picture. That's what I was think but two heads are better then one.

    Thanks for the advice, take care.

  4. #4

    Re: Would the AX-12W be better then AX-18A for the PhanomX Hexapod MarkII

    The math is very simple. Distance of lever, times force on lever, equals torque. The robot weighs perhaps 1-2 kg depending on payload, which means the distance of your leg span can be a whopping 1-2 centimeters before stalling out. That's smaller than the size of the servo itself! And, ideally, you should design for a normal load of 1/4 to 1/5 of the stall torque.
    The AX-12W are intended only for rolling applications, where the torque needed is much smaller, but speed (in RPM) can be useful.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX Hexapod Kit
    By SuperMiguel in forum Projects For Request and/or Sale
    Replies: 12
    Last Post: 12-29-2013, 09:36 PM
  2. My PhantomX Hexapod
    By Gilrock in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 09-26-2012, 02:23 PM
  3. Hexapod V1-TR
    By amorfy in forum Project Showcase
    Replies: 11
    Last Post: 05-27-2011, 02:11 AM
  4. Cad Design for Hexapod
    By epsilonorion in forum Robotics General Discussion
    Replies: 1
    Last Post: 10-03-2010, 06:17 PM
  5. News/Announcement micromagic hexapod kit MSR-H01
    By mdenton in forum Humanoids, Walkers & Crawlers
    Replies: 33
    Last Post: 10-04-2008, 05:37 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •