Results 1 to 4 of 4

Thread: Hexapod MK2 - Servo not responding as it should . Dead zone, and wrong readings.

  1. #1

    Hexapod MK2 - Servo not responding as it should . Dead zone, and wrong readings.

    Hi, I received my Hexa MK2, a few days ago. all god,
    I already followed the assembly guide.

    1- Uploaded the sketch for MK2, and
    on the STARTUP POSITION, one leg goes all cramped, the Servo ID 9 , is not going to the expected position as all the other legs.

    2- Uploaded the Sketch of PyPose, to do some debuging.
    I can see that ALL SERVOS ID are OK (1 to 18), tested one by one, doing read pose, and set pose for different range of values.

    3- Servo ID 9, is out of range shows 1023 in the same position all the others servos show 0, and jumps from 1000 to 500 when moving the servo by hand,
    When initialazed the MIRROR SERVO on the other leg, goes to 640, in the same position the servo 9, shows 60 when captured the pose .

    any ideas ?
    Which tool I should use to debug this, or rewrite all the settings on the servo 9. ?
    All this test, were done , removing the xbee on the arbotix, connected FTDI to USB cable, using Ubuntu 12.04, Arduino 1.0.5,
    the errors on the Servo 9, exist with Sketch PyPose, and also the mark2 skecth
    best regards
    Eze

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: Hexapod MK2 - Servo not responding as it should . Dead zone, and wrong readings.

    Did you verify you installed the servo in the correct orientation and with the horn pointing in the correct direction when attached to the frame? It sounds like the horn was rotated from its correct orientation when screwing the frame into the horn, and/or the servo was rotated such that the horn rotates in the opposite direction of how it should.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: Hexapod MK2 - Servo not responding as it should . Dead zone, and wrong readings.

    Hi, thanks for the fast reply,
    all looks good, as orientation, and horn pointing, is the only servo misbehaving.
    I will deattach, and check all this, if there is another position I will try it.

  4. #4

    Re: Hexapod MK2 - Servo not responding as it should . Dead zone, and wrong readings.

    THANK YOU VERY MUCH.
    SOLVED.
    I disconnected the servo, the horn was rotated, I moved it a little bit, re attached, and now is all good.
    As I uploaded the firmware MARK2 and all when to the rigth position.
    THANK YOU for the fast help

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Twitch - My 3 Servo Hexapod
    By Gertlex in forum Project Showcase
    Replies: 39
    Last Post: 07-16-2015, 02:17 PM
  2. Question(s) Dynamixel AX-12A not responding
    By patinam in forum DYNAMIXEL & Robot Actuators
    Replies: 6
    Last Post: 03-04-2013, 02:41 PM
  3. Servo torque required for hexapod
    By Fatfrank69 in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 02-19-2013, 06:08 PM
  4. Question(s) Just another hexapod servo controller thread
    By Croc in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 04-05-2011, 10:55 PM
  5. Contest Entry Donna The Dead Bot
    By Rodger Cleye in forum Project Showcase
    Replies: 5
    Last Post: 11-02-2009, 09:34 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •