Results 1 to 2 of 2

Thread: motion and measurement models for Kinect

  1. #1
    ajp Guest

    motion and measurement models for Kinect

    Hi
    I would like to implement SLAM with the Kinect for a research project. I am not sure which motion and measurement models to apply though. Would anyone be able to recommend which models I can apply to the Kinect or a good place to start. I will be using ROS Fuerte. Thank you



  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    128

    Re: motion and measurement models for Kinect

    Seeing as the kinect doesn't move on it's own, I have no idea why you would define a kinect-based motion model.

    As for measurement model, it's pretty similar to a stereo camera. These are two resources I know of that have some actual numbers:
    http://www.ros.org/wiki/openni_kinect/kinect_accuracy
    http://ros.org/wiki/kinect_calibration/technical

    -Fergs

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Kinect 2 or Capri 1.25
    By Gort in forum Sensors
    Replies: 9
    Last Post: 03-07-2013, 05:17 PM
  2. Kinect Fusion
    By billyzelsnack in forum Robotics General Discussion
    Replies: 1
    Last Post: 08-12-2011, 12:23 AM
  3. SMPS2Dynamixel and Kinect?
    By Pi Robot in forum Power
    Replies: 7
    Last Post: 02-24-2011, 01:35 PM
  4. Question(s) Motion sequencing in RoboPlus Motion?
    By jarred in forum Software and Programming
    Replies: 4
    Last Post: 05-07-2010, 08:54 AM
  5. Just For Fun Lighter side of Robot models (SFW&NSFW)
    By ashwinmudigonda in forum Off Topic
    Replies: 6
    Last Post: 05-02-2008, 08:15 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •