Results 1 to 8 of 8

Thread: Help finding servo potentiometers

  1. #1
    Join Date
    Sep 2012
    Location
    Alameda, CA
    Posts
    31
    Rep Power
    22

    Help finding servo potentiometers

    I'm looking for a servo potentiometer and I can't seem to find anything remotely close to it on Mouser or DigiKey. Those website are nebulous and packed dense with information. Could someone point me the right direction??

    I'm looking for a potentiometer with the smallest dimension down the axis of the shaft, the diameter or width height is not too important.

    The application is to use it as a rotary sensor. I could purchase cheap servos and rip it out of them, but that just seems wasteful.




    Thanks!!!

    -Alonso

  2. #2
    Join Date
    Feb 2012
    Location
    Sydney, Australia
    Posts
    364
    Rep Power
    33

    Re: Help finding servo potentiometers

    Would you be willing to consider an encoder instead of a pot?

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,282
    Images
    27
    Rep Power
    275

    Re: Help finding servo potentiometers

    Digikey -> Sensors, Transducers -> Position Sensors - Angle, Linear Position Measuring
    All angular and rotary sensor types.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  4. #4

    Re: Help finding servo potentiometers

    If you absolutely need a potentiometer, you could try a "trimmer" which has no shaft, just a cross in the center of the wiper.
    However, if the point is to sense position, I would highly recommend using some kind of optical or magnetic absolute encoder.
    And if the point is to sense velocity, a quadrature encoder (optical or Hall) would be sufficient.

  5. #5
    Join Date
    Feb 2012
    Location
    Sydney, Australia
    Posts
    364
    Rep Power
    33

    Re: Help finding servo potentiometers

    A trimmer could be an option, but if you do go with one be aware that they usually have very short rotational lifespans since they're normally meant to be set then never adjusted again.

  6. #6
    Join Date
    Sep 2012
    Location
    Alameda, CA
    Posts
    31
    Rep Power
    22

    Re: Help finding servo potentiometers

    I actually purchased trimmer pots from DigiKey only to find out that like Th232 said the life cycle for most of them were 500 turns...

    I have thought about using a magnetic rotary encoder, but it sounded like more complex electronics that I've done so far, but it might be a good project to learn this stuff.

    I found AtonB's servo hack's tutorials and although it seems that his www.01mech.com website is down, I found these files:

    https://code.google.com/p/zosupermodified/

    I don't know how to use Eagle schematics software but I'm going to start by looking into CadSoft Eagle. Is this a good software to use?

  7. #7
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,282
    Images
    27
    Rep Power
    275

    Re: Help finding servo potentiometers

    Eagle is pretty nice, but very expensive if you need more layers or larger boards than the 'freeware' version permits. I have not really been doing much pcb design recently, so I have not had the incentive to change over to Kicad or gEDA.

    For some reason I remember the AX-12+ encoder being blue, but that may just be my brain making up more crap. I bought a couple of these for the laser range finder that I never finished and never got a chance to make a board for them. All you are supposed to need is a 3V regulator, a couple decoupling capacitors, and an ADC pin on your microcontroller.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  8. #8

    Re: Help finding servo potentiometers

    You can buy ready-made optical encoders that can mount straight to a shaft. There's typically a "reader" part and a "disc" part.
    The main concern there would be size -- I'm not sure you can get off-the-shelf miniature parts -- and perhaps price, if you're very price sensitive.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Interesting Hack servo v3.00 - Get full PID position and speed control from your hobby servo
    By Antonb in forum Mechanics / Construction
    Replies: 20
    Last Post: 06-27-2010, 10:24 AM
  2. How to use a wck1111 servo (or any serial servo)
    By kiwibrisa in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 04-28-2010, 12:56 AM
  3. Replies: 11
    Last Post: 02-26-2010, 10:57 AM
  4. Hack your Servo V1.00: Make a linear actuator using a hobby servo
    By Antonb in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 01-15-2010, 01:43 PM
  5. Student Project II (finding the parts)
    By csdude in forum Rovers
    Replies: 22
    Last Post: 06-03-2008, 08:55 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •