Results 1 to 5 of 5

Thread: 2 DoF Quad gait

  1. #1
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    40

    Question 2 DoF Quad gait

    Okay guys, all I'm asking for is information on the best ways to create a gait for a 2 DoF Issy Dunn Yet style mech. I will be using AX-12A's for servos.

    I have asked Lnxfergy, but have gotten no reply.

  2. #2

    Re: 2 DoF Quad gait

    I only know of one way. The "ankle" lifts up/down, and the "hip" does locomotion. This leads to foot sliding.

    Start with FL and RR hips turned "backwards" and FR and RL hips turned "forwards" and all feet down.

    Now, FL and RR ankles turn "up"
    Then, the FL and RR hips servos turn forward, and the FR and RL servos turn backward. This uses the FR/RL pair to push the bot forward.
    Now, FL and RR ankles turn "down" and FR and RL ankles turn "up"
    Then, FL and RR hip servos turn backward, and FR and RL turn forward. This uses FL and RR pair to push the bot forward.
    Now, repeat from top.

    Turning "up" should probably be less than an inch upwards, because you will likely "skate" on one of those two "up" legs, and you want to not tip too much backwards/forwards during this movement.

    It may be possible to twist the ankles that are in contact with the ground to stay at a relative distance sideways from the bot center, and instead move the body up/down, to avoid foot sliding (instead getting body up/down motion) but I haven't worked out the math for that or know anything about whether that will actually be an improvement in capability.

  3. #3
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    40

    Re: 2 DoF Quad gait

    Yeah, I used that technique with M-O in that junk walking video. I finally realized that if you added surface area to the foot (make it a square or larger circle, instead of a little peg) that the bot might walk without foot sliding.

  4. #4

    Re: 2 DoF Quad gait

    the bot might walk without foot sliding
    The only way that can mathematically work is if you also alter the contact angle with the ground at the same time, and thus raise/lower the body at the same time. And with a "spike" foot, that should be equally possible -- as long as you can get sufficient friction between foot and ground.

    The reason I say this is because, if you don't tilt the foot while sweeping the hip front-to-back, then the arc of the foot contact point around the hip joint is a pure circle. And the relative X position of the foot will then be leg-length times sin(angle) (where angle is 0 when straight forward.) This is what forces (sideways) sliding.

    So, if a 2dof foot can reach forward to point X with "full extent," and you can then compensate the radius of the leg while it's sweeping, by tilting the foot down (and thus moving the body up,) then you should be able to avoid sideways foot sliding. I have not tried it, though.

  5. #5
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    40

    Re: 2 DoF Quad gait

    Oh, okay. I didn't know what you were meaning by foot sliding. I meant the bot tilting forward and the foot that is lifted on the front ending up being a skid plate.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Bioloid Developing a Walking Gait
    By kambozza in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 01-05-2013, 06:27 AM
  2. My Hexapod tripod gait
    By sa3don in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 09-22-2012, 02:29 AM
  3. Gait implementations
    By mblackwolf in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 10-21-2011, 11:24 AM
  4. Just For Fun My Quad
    By blastdog in forum Project Showcase
    Replies: 6
    Last Post: 06-25-2011, 08:07 AM
  5. Question(s) Hexapod Fast Gait legs slap
    By DTM in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 03-09-2011, 01:07 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •