Page 2 of 2 FirstFirst 12
Results 11 to 14 of 14

Thread: phantom AX12 speed control?

  1. #11

    Re: phantom AX12 speed control?

    no it does not work correctly when using stock code the same problem occur

  2. #12

    Re: phantom AX12 speed control?

    Sounds like you have a mechanical problem then.

  3. #13
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    146

    Re: phantom AX12 speed control?

    Verify your servo ID installation, there is a diagram in the assembly guide.

    If it's not walking straight when using the stock code/commander, then you most likely have a problem with servo ID(s) being installed in the incorrect spot.

  4. #14

    Re: phantom AX12 speed control?

    Also as I have mentioned in a few different threads. When things are not working correctly, I will use my AX12 test and have it check each of the servos to see if it can talk to each one...

    https://github.com/KurtE/AX12_Test

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. modeling of phantom ax12 hexapod?
    By abdelrahman in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 04-27-2013, 04:10 PM
  2. Question(s) phantom ax12 stopped working
    By abdelrahman in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 02-12-2013, 07:12 PM
  3. Hardly Used Phantom X Turret Kit - AX12
    By rad1424 in forum Garage Sale
    Replies: 1
    Last Post: 03-05-2012, 11:08 PM
  4. Control of Photon Speed 20 Motor
    By DaniA in forum Robotics General Discussion
    Replies: 5
    Last Post: 03-14-2010, 08:51 PM
  5. Wifi to Control AX12 Mech??
    By DC Robotic in forum Robot Computers
    Replies: 8
    Last Post: 10-24-2009, 09:26 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •