Hi. I've been recently introduced to Variable Stiffness Actuators and Force/Impedance control in robot manipulators arms. For this pourpose, a feedback of the torque (or equivalently the current) is needed. Dynamixel MX-106 seems to provide current measurements, however, in the tech specs it says:
<<Notes: Current load is inferred from the internal torque value, not from Torque sensor etc. For that reason, it cannot be used to measure weight or torque; however, it must be used only to detect which direction the force works.>>
(http://support.robotis.com/en/produc...ies/mx-106.htm)
A very similar question was already stated here: http://forums.trossenrobotics.com/sh...rrent-feedback
However, the response is not enough for me. Has anyone tried contolling a Dynamixel servo in force/torque? Is there any not too complex way to measure externally the current? I do not require too much accuracy in the measurements.
Thanks in advance.
Bookmarks