Results 1 to 3 of 3

Thread: ROS motor controller

  1. ROS motor controller

    What do you guys use to control motors from ROS? hardware and software

  2. Re: ROS motor controller

    was thinking to use the http://www.pololu.com/product/708/ and the arbotix but not sure

  3. #3
    Join Date
    Dec 2013
    Location
    Redondo Beach, California
    Posts
    5
    Rep Power
    21

    Re: ROS motor controller

    Look here. ROS on Beagal Board controlling a DC motor via h-bridge. Looks like using an INU to control the speed. I've not looked at the code. https://github.com/vmayoral/bb_dc_motors

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Newbie! Control a 12V DC Motor using 1061 Servo Controller and L298 Dual H-Bridge Motor Driver
    By dmar in forum Arbotix, Microcontrollers, Arduino
    Replies: 10
    Last Post: 09-05-2013, 02:32 PM
  2. Contest Entry PID Velocity DC Motor Controller
    By Upgrayd in forum Project Showcase
    Replies: 0
    Last Post: 12-31-2010, 10:46 AM
  3. Question(s) Motor Controller. Do I need a servo controller too?
    By kankatee in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-14-2008, 10:03 AM
  4. Question(s) Motor controller ?'s
    By sthmck in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 11-06-2008, 03:29 PM
  5. Question(s) Motor Controller
    By sthmck in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 09-15-2008, 05:37 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •